Passive Components
  • Technologies
  • More
Passive Components
Polls Will Embedded Passive Components Obsolete Surface Mounted Passives?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 25 Aug 2019 11:22 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 1194 views
  • Likes 1 like
  • Comments 4 comments
Related
Recommended

Will Embedded Passive Components Obsolete Surface Mounted Passives?

Embedded passive components are buried within the PCB substrate during fabrication. They can offer benefits such as lower costs, improved electrical performance, increased packaging density, less parasitic losses, less cross talk, improved signal transmission, and more.

 

Here's the question: Will Embedded Passives Components Obsolete Surface Mounted Passives?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +3
    I doubt that will ever be the cheapest way to produce PCBs and that's what drives a large amount of production. I can see it getting used for high end stuff where size or performance is paramount, but…
  • michaelkellett
    michaelkellett over 7 years ago +3
    The chemistry of making fibreglass/copper pcbs is not compatible with that for making semiconductors or most passive components - so you might end up embedding small, pre-tested and manufactured parts…
  • dougw
    dougw over 7 years ago +2
    Interesting question. The number of designs that use this technique will increase as costs come down and the advantages start to outweigh the costs. It isn't clear to me how much density would increase…
  • dougw
    dougw over 7 years ago

    I think we will see a lot more electrical components and interconnections embedded directly in 3D printed mechanical structures - sometimes doing away with PCBs altogether.

    I wonder if electrical components will become available in special form factors for assembly into 3D printed structures, or if normal SMT form factors are adequate.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago

    The chemistry of making fibreglass/copper pcbs is not compatible with that for making semiconductors or most passive components - so you might end up embedding small, pre-tested and manufactured parts in the pcb. For most applications this sounds like increased cost and additional problems for very little gain.

    There may be special applications where there is a big performance advantage and it may happen there.

    Current applications are mainly chip on board (for low cost, low reliability) or very low grade resistors for mass production.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago

    I doubt that will ever be the cheapest way to produce PCBs and that's what drives a large amount of production. I can see it getting used for high end stuff where size or performance is paramount, but that's not the bulk of electronics.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago

    Interesting question. The number of designs that use this technique will increase as costs come down and the advantages start to outweigh the costs. It isn't clear to me how much density would increase with this technology since the interior of PCBs is already congested with many trace layers.

    However, not only does the process need to be cheap, CAD tools will have to be developed and available at low cost to allow a new generation of students to drive demand for the technology before it has a chance to really take off.

    I can imagine the day when chips have BGAs on both top and bottom of the chip.....