Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech 12.5 Trillions of gallons of fuel wasted a year
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
  • Author Author: Eavesdropper
  • Date Created: 8 Mar 2011 8:03 PM Date Created
  • Views 1055 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • biofuels
  • on_campus
  • algae
  • university
  • biodeisel
  • innovation
Related
Recommended

12.5 Trillions of gallons of fuel wasted a year

Eavesdropper
Eavesdropper
8 Mar 2011
image
wastewater facility
 
Newcastle University in the U.K. is making new with their latest claim. The “United States flushes 12.5 Trillion gallons of energy down the drain.” They are referring to biofuels in sewage. Newcastle’s Elizabeth S. Heidrich says, “Instead of just processing and dumping this water, we suggest that in the future treatment facilities could convert its organic molecules into fuels, transforming their work from an energy drain to an energy source. Based on our research, we estimate that one gallon of wastewater contains enough energy to power a 100-watt light bulb for five minutes.” A quick internet search offers up thousands of "make your own biofuels at home" links. There are many vehicles that can run on the biofuel, biodiesel. With an ample source of sewage everywhere, biofuels is an option worth exploring. Thanks Newcastle.
 
image
micro-algae
 
One method of using wastewater to generate a biofuel from waste water is from algae. Researchers at the Rochester Institute of Technology, for example, use microalgae as a "renewable feedstock" in the process of making biodiesel. As the algae absorbs some of the wastewater elements they produce a tiny bit of biodiesel. One of the researchers, Jeff Lodge, explains further, " Algae will take out all the ammonia—99 percent—88 percent of the nitrate and 99 percent of the phosphate from the wastewater — all those nutrients you worry about dumping into the receiving water. In three to five days, pathogens are gone... We can start a new batch of algae about every seven days. It’s a more continuous source that could offset 50 percent of our total gas use for equipment that uses diesel." The team eventually extracts the lipids from the single cell algae Scenedesmus to make the biodiesel. Currently the team is only producing 100 gallons at a time, but hope to expand to 1000 by spring. Apply this  technique to trillions of gallons, and offseting fuel shortages it will. Good luck R.I.T.
 
Eavesdropper
  • Sign in to reply
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    I will admit, I have recently become quite passionate about recycling. I carried a plastic bottle from the beach, to a movie theatre, to a park, around Chicago, just to recycle it at home. I think it has come from writing about so many alternative energy projects happening in the world. I am all for waste water recycling, but it sounds like a dirty job.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 15 years ago

    I for one will be much happier when people stop thinking of "waste" material as something to dump and begin to realize the incredible opportunity that exists if we would "mine" the material instead.  I am encouraged that some of my local farmers are using the left over sludge as free fertilizer for their crops.  I think that is the key to enhancing reuse, is to help people understand that it has "value".  Then they will less likely to want to just dump it somewhere.

     

    Thanks,

    DAB