Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech Fresh to saltwater mixing for power
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
  • Author Author: Eavesdropper
  • Date Created: 30 Mar 2011 7:23 PM Date Created
  • Views 1792 views
  • Likes 2 likes
  • Comments 3 comments
  • research
  • dit
  • eavesdropper:dit
  • river
  • energy_harvast
  • saltwater
  • water
  • on_campus
  • renewable
  • university
  • power
  • innovation
Related
Recommended

Fresh to saltwater mixing for power

Eavesdropper
Eavesdropper
30 Mar 2011
image
 
Where fresh water meets saltwater there is a potential to harvest energy. Stanford University researchers have developed a device that can use this use the mixing of the two water types and pull out more energy that they put in. A container holds fresh water, with positive and negative electrodes at either end, is charged and then submerged in saltwater. The device allows the two waters to mix. Since  saltwater contains more ions of sodium and chlorine, the electrical potential between the electrodes increases.
 
Researcher Yi Cui elaborates, "The voltage really depends on the concentration of the sodium and chlorine ions you have. If you charge at low voltage in freshwater, then discharge at high voltage in sea water, that means you gain energy. You get more energy than you put in."
 
His idea is to place these devices when rivers, or other fresh water supplies, meet saltwater bodies, like the ocean. He claims that is every river mouth, estuaries, were tapped, 13% of the worlds electricity need would be met. (2 terawatts)
 
The battery could be 85% efficient, says Cui. To achieve this rating, the positive electrode is made of nanorods of manganese dioxide. This allows more surface area for the sodium ions to interact, move in and out, and speed up the process. This is not the first time electricity has been produces from the mix of saltwater and fresh water. However, this time both sodium and chlorine ions are used to generate power.
 
The next step for the team is to try this process with sewage water.
 
For the record, funding for Yi Cui's project has come from The King Abdullah University of Science and Technology (KAUST) and the U.S. Department of Energy.
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 15 years ago

    This concept gives me an idea on how to use the waste water from my water softner to potentially generate power.  I will have to give this idea more thought, but this is indeed very interesting.

    It also reminded my of a trip I made to Alaska where I could look out and actually see the salt/fresh water line stretching for miles where the Stikine river flowed into the North Pacific.  It was an amazing sight.

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 15 years ago

    This concept gives me an idea on how to use the waste water from my water softner to potentially generate power.  I will have to give this idea more thought, but this is indeed very interesting.

    It also reminded my of a trip I made to Alaska where I could look out and actually see the salt/fresh water line stretching for miles where the Stikine river flowed into the North Pacific.  It was an amazing sight.

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    Dab,

     

    Any developments on your water softener alternative energy project?

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 15 years ago in reply to Eavesdropper

    I have some containers, some tubing, and some connectors, but this project is on hold as I just got the parts I ordered to build the Macrophotography lights.  I will get to this one in time and I hate to think of throwing the used salt water down the drain if I can use it to do something more useful.

    I will keep you posted.

    Thanks,

    DAB