Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech High-performance capacitor could lead to more efficient technology
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
  • Author Author: Eavesdropper
  • Date Created: 27 Jan 2011 1:24 AM Date Created
  • Views 543 views
  • Likes 0 likes
  • Comments 0 comments
  • capacitor
  • alternative_energy
  • supercapacitor
  • ultracapacitor
Related
Recommended

High-performance capacitor could lead to more efficient technology

Eavesdropper
Eavesdropper
27 Jan 2011
image
 
In order to develop next-generation electric vehicles, solar energy systems, and other clean energy technologies, researchers need an efficient way to store the energy. One of the key energy storage devices for these applications and others is a supercapacitor, also called an electric double-layer capacitor. In a recent study, scientists have investigated the possibility of using a material called zeolite-templated carbon for the electrode in this type of capacitor, and found that the material’s unique pore structure greatly improves the capacitor's overall performance. Recently, scientists have been testing materials with pores of various sizes and structures to try to achieve both quick ion transport and high adsorption ion density. But the two requirements are somewhat contradictory, since ions can travel more quickly through larger nanopores, but large nanopores make the electrode density low and thus decrease the adsorbed ion density. The scientists decided to use zeolite-templated carbon to seemingly overcome this problem. Zeolite-templated carbon consists of nanopores that are 1.2 nm in diameter and that have a very ordered structure. The nanopores’ small size makes the adsorbed ion density high, while the ordered structure (described as a diamond-like framework) allows the ions to quickly pass through the nanopores. In a previous study, the researchers showed that zeolite-templated carbon with nanopores smaller than 1.2 nm cannot enable fast ion transport, suggesting that this size may provide the optimal balance between high rate performance and high volumetric capacitance. In tests, the zeolite-templated carbon’s properties exceeded those of other materials, demonstrating its potential to be used as an electrode for high-performance electric double-layer capacitors. For more information please visit: http://pubs.acs.org/doi/abs/10.1021/ja108315p
 
Eavesdropper