Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech Honda Soltec announces new efficient CIGS-based thin film solar cell
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
  • Author Author: Eavesdropper
  • Date Created: 31 Jan 2011 7:34 PM Date Created
  • Views 624 views
  • Likes 0 likes
  • Comments 0 comments
  • research
  • enery_harvast
  • honda
  • solar
  • solar_cell
Related
Recommended

Honda Soltec announces new efficient CIGS-based thin film solar cell

Eavesdropper
Eavesdropper
31 Jan 2011
image
 
Honda Soltec Co., Ltd. will this year release a new thin-film solar cell with an even more compact design than the current model to allow efficient installation on a wide range of roof shapes. The prototype manufactured using existing Honda Soltec equipment achieved a module conversion efficiency of 13.0%. Honda is working to further improve module conversion efficiency as it brings the product to market. Honda’s independently developed CIGS thin-film solar cells require little energy in the manufacturing process, further contributing to environmental preservation. Honda will continue to contribute to the preservation of the global environment by developing thin-film solar cells that respond to market needs, thereby promoting further widespread use. The performance of the photosensitive CIGS layer has been improved and the surface area of the surrounding frame and other non-photosensitive portions reduced, resulting in approx. 10% increase in module conversion efficiency compared to the current model. This results in more power generated from the same installed surface area. The new model is more compact, with only approx. two-third the module surface area of the current model, allowing it to be installed in limited space on a wide range of roof shapes. This will facilitate the efficient installation of more thin-film solar cells in a variety of locations. For more information visit: http://translate.google.com/translate?hl=en&sl=ja&u=http://www.honda.co.jp/soltec/&ei=6O5GTfbSLMP98Ab1-M2eAg&sa=X&oi=translate&ct=result&resnum=1&ved=0CCUQ7gEwAA&prev=/search%3Fq%3Dhttp://www.honda.co.jp/soltec/%26hl%3Den%26client%3Dfirefox-a%26hs%3DhsI%26rls%3Dorg.mozilla:en-US:official%26prmd%3Divns

Eavesdropper