Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech Solar-thermal water heater for the home
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
  • Author Author: Eavesdropper
  • Date Created: 16 Mar 2011 7:27 PM Date Created
  • Views 1033 views
  • Likes 1 like
  • Comments 1 comment
  • alternative_energy
  • solar_thermal
  • energy_harvast
  • alternative
  • heat_energy_transfer
  • renewable
  • home
  • solar
  • automation
  • innovation
Related
Recommended

Solar-thermal water heater for the home

Eavesdropper
Eavesdropper
16 Mar 2011
This video is unavailable.
You don't have permission to edit metadata of this video.

 
Solar thermal has come to residential customers directly. SolarTron Energy Systems Inc,  a division of EG Energy Controls, in an attempt to enter the alternative energy industry with the "SolarBeam Solar Concentrator." This device is being marketed as a efficient way to heat water. In fact, it is 262% more efficient than hot water panels, and 98% more efficient than evacuated tube technology, according to SolarTron. The SolarBeam can provide 10kW/hour up to 13kW/hour (44,000 BTUs) of heat throughout a sunny day, and can even run air-conditioning using and absorption chiller. As of 2011, the SolarBeam will also produce 4kW/hour of electricity. The SolarBeam sits on top of a 12 foot pole, or on a flat roof. The system also tracks the sun to provide the most optimal performance. The systems account for seasonal changes, and can withstand the element, and 140km/hour winds.
 

If you do not mind the 1980's satellite dish look in your backyard, this is a great options for you. However, it will take up to 6 years for the device to pay for itself. After that, it is all profit.
 

Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 15 years ago

    I like the results, but the big dish is a major drawback.  Plus, I live in an airport flight path and can see where that could cause some nasty problems at certain sun angles.

    Other than that, a very interesting system.

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 15 years ago

    I like the results, but the big dish is a major drawback.  Plus, I live in an airport flight path and can see where that could cause some nasty problems at certain sun angles.

    Other than that, a very interesting system.

    Thanks,

    DAB