Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech The world’s largest wind farm is up and running in the UK
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
  • Author Author: Catwell
  • Date Created: 25 May 2017 8:49 PM Date Created
  • Views 5687 views
  • Likes 3 likes
  • Comments 20 comments
  • turbine
  • industrial
  • green
  • alternative energy
  • cabeatwell
  • uk
  • wind farm
  • innovation
Related
Recommended

The world’s largest wind farm is up and running in the UK

Catwell
Catwell
25 May 2017

image

This wind farm has turbines that are 640 feet tall with 262 foot long blades built by Dong Energy. These turbines are bigger than some skyscrapers (Image via MHI Vestas)

 

The world’s largest wind farm is now up and running in the UK. The 32 huge turbines built by Danish company Dong Energy are housed in Liverpool Bay. The turbines boast a greater height than some skyscrapers standing at 640 feet tall and equipped with 262-foot long blades, which can produce eight megawatts of power. This is actually the first time 8MW turbines have been used for commercial purposes. Their power is supposed to be so great the company claims a single revolution of the blade can power one house for 29 hours.

 

The 32 new turbines are an extension of the Burbo Bank wind farm that was built over a decade ago. This latest addition makes Britain a world leader in wind farm technology. Because of subsidies, friendly regulation, and their maritime past, the UK have installed more offshore wind power than any other country in the world. This latest addition along with their existing structures give them the capacity of 5.3 GW, that’s enough electricity to power 4.3 million homes. And it doesn’t stop here; there are eight more projects in the works.

 

But to keep receiving support for the tech from the government, the industry has to keep cutting costs. This in part is why Dong Energy opted to build such large turbines. You would think the cost to maintain these things would be high considering how big they are. Believe it or not, these large turbines are cheaper to build and maintain since each tower and blade needs a foundation. In the end, it’s cheaper than maintaining lots of small turbines. The company hopes this leads to offshore wind power that’s bigger, better, and cheaper than before.

 

These wind turbines greatly benefit the UK, but they’ve still come under fire for not having enough parts made in Britain. Dong Energy doesn’t exactly help matters; they don’t reveal what how much of the Burbo Bank extension is UK built. Fortunately, half of the blades are made at MHI Vesta’s Isle of Wight factory. On the other hand, these farms create new jobs and offer residents a long term career.

 

Still, you can’t argue with results, and the UK seems pretty pleased overall. There are more wind turbine projects scheduled for the future; these will also use 8MW turbines. It seems the UK is set on keeping its reputation as a world leader in windfarm technology. They’re certainly ahead of the US, which recently installed its first offshore wind farm.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to mcb1 +2
    Here's a link with some plausible calculations: https://www.forbes.com/sites/quora/2016/09/22/we-could-power-the-entire-world-by-harnessing-solar-energy-from-1-of-the-s… MK
  • DAB
    DAB over 9 years ago +1
    I am curious. Does anyone else see the skull shaped cloud behind the wind towers? DAB
  • michaelkellett
    michaelkellett over 9 years ago in reply to e14phil +1
    Subsidies always distort things and now we have huge industries dependent on them - it's not a surprise that they defend them. I'd like to see a complete end to subsidies in energy supply - then we would…
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    I live in the UK and I'm not pleased.

    These ******* windmills are massively subsidised - so called "green" incentives add, on average, over £100 to each household energy bill  and this is likely to rise to a great deal more in the next few years.

    Scotland, where I live, is plastered with the hideous things, ruining the countryside, making electricity when we don't want it and often not when  we do.

    We aren't  a leader in the technology to make the stupid things, Dong is. We're just the mugs who pay for them.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

     

    ... making electricity when we don't want it and often not when we do...

     

     

     

    That thought crosses my mind every frosty morning in winter time when you look at all those wind turbines standing motionless whilst there is a very high demand for energy to heat homes and work places.

     

    It perhaps needs more investment in pumped storage hydro schemes to act as a buffer between generation and consumption, but large scale hydro apparently turns out not the be very green either.

     

    That then brings me onto a second thought which is what happens when the natural gas finally runs out. All of a sudden in winter you then have an extra 20kW or so load per home placed on the electricity supply grid as people switch over from gas to electricity for heating, which I suspect the existing electricity supply network can't currently deliver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 9 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

     

    ... making electricity when we don't want it and often not when we do...

     

     

     

    That thought crosses my mind every frosty morning in winter time when you look at all those wind turbines standing motionless whilst there is a very high demand for energy to heat homes and work places.

     

    It perhaps needs more investment in pumped storage hydro schemes to act as a buffer between generation and consumption, but large scale hydro apparently turns out not the be very green either.

     

    That then brings me onto a second thought which is what happens when the natural gas finally runs out. All of a sudden in winter you then have an extra 20kW or so load per home placed on the electricity supply grid as people switch over from gas to electricity for heating, which I suspect the existing electricity supply network can't currently deliver.