Power & Energy
  • Technologies
  • More
Power & Energy
Alt Energy Solutions & Tech Throw away hydrogen fuel cell charger, 5Wh for your mobile device
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
  • Author Author: Catwell
  • Date Created: 5 Oct 2012 7:06 PM Date Created
  • Views 1510 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • alternative_energy
  • japan
  • prototype
  • alternative
  • rohm
  • power_station
  • battery
  • cabeatwell
  • fuel_cell
  • renewable
  • power
  • hydrogen_for_power
  • energy_storage
  • innovation
Related
Recommended

Throw away hydrogen fuel cell charger, 5Wh for your mobile device

Catwell
Catwell
5 Oct 2012

imageimage

 

Here a simple idea that may save your hide but may conflict with your long-term desire to save the planet. The Rohm portable charger allows you to charge your phone on the go using one of the two devices they have developed: a phone case made for the iPhone or a standalone USB charger that connects to other handheld devices. The only downside is that it can only be used once.

 

 

The fact that the neat charger will end up in the landfill should not be the focus of the conversation. Rohm generates this electricity using a non-toxic hydrogen fuel cell that allows for such small devices. The stylish iPhone case elongates the phone but adds little bulk while the standalone unit is about the size of your cell phone itself.

 


image

 

The device generates electricity by exploiting the hydrogen that results from a reaction with thin sheet of resin-solidified calcium compound. The hydrogen then combines with the polymer electrolyte material to generate 5Wh of electricity.

 

 

Although the plastic isn’t going anywhere, Rohm says the device is entirely non-toxic so no worries about throwing it away. They expect customers will buy them as a backup or for emergencies claiming it will last for 20 years, as long as that calcium compound sheet remains sealed. Rohm has also built a 200W version of the charger intended for bigger applications like laptops or other peripherals that lasts for up to 4 hours.

 

 

No mention of price just yet as the device will hit the shelves in 2013, but it should reflect its disposable downside. Similar reusable devices are much bigger and very pricey. It's a shame that we have to make decisions with our wallets in mind instead of the planet but hopefully Rohm develops some sort of reusable form soon.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I am sure that it would not take much more engineering to develop a reusable/refillable fuel cell.

    The last thing the planet needs is another throw away product.  I would rather see someone build a hand crank or foot crank device to recharge these devices.  People need more exercise, not one more thing to put into our land fills.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Although emergency use is the purpose of this device, I am on your side of thought. Tech of this caliber should not be thrown away.

     

    However, I am sure it is reusable.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Although emergency use is the purpose of this device, I am on your side of thought. Tech of this caliber should not be thrown away.

     

    However, I am sure it is reusable.

     

    Cabe