Power & Energy
  • Technologies
  • More
Power & Energy
Blog Largest Solar Plant Facility Under Construction in Illinois
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 1 Oct 2024 7:03 PM Date Created
  • Views 1256 views
  • Likes 6 likes
  • Comments 1 comment
  • alternative_energy
  • illinois
  • contruction
  • usa
  • cabeatwell
  • solar
  • innovation
Related
Recommended

Largest Solar Plant Facility Under Construction in Illinois

Catwell
Catwell
1 Oct 2024

image

(Image Credit: Michael_Pointner/pixabay)

Swift Current Energy has started building the Double Black Diamond Solar Facility, the largest solar project in southern Illinois. Once complete, the solar facility expects to produce 800 megawatts of electricity---sufficient for powering 100,000 homes annually. It also has the potential to slash carbon dioxide emissions by one million tons per year.  Power will be distributed to several facilities, such as O’Hare International Airport and Loyola University Chicago.

“We are proud to be home to one of the largest clean energy projects in the nation. The Double Black Diamond Solar project brings significant economic benefits to our community, contributing $100 million in tax revenue and supporting hundreds of jobs. This project is a win for both our community and the environment,” said Sangamon County Board Chairman Andy Van Meter

In addition, the Double Black Diamond Solar facility could become a big economic boost for the local community. According to officials, the project expects to generate $100 million in tax revenue and create hundreds of jobs through the facility’s construction and operational phases.

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • robogary
    robogary over 1 year ago +1
    Neat story - I searched for details about the "american" solar panels, provider of the control system, DCS hardware vendor, power conversion hardware vendor, etc. Did see the solar panels used are the…
  • robogary
    robogary over 1 year ago

    Neat story - I searched for details about the "american" solar panels, provider of the control system, DCS hardware vendor, power conversion hardware vendor, etc.   Did see the solar panels used are the ones with cells on both the front and underside. The claim to fame is the panel aiming system to tilt the panels to stay out of the shadow of the panel row in front of it, rather than stay perpendicular to the sunshine. https://www.nextracker.com/blog/energy-insights/closing-the-reality-gap-optimizing-solar-plants-performance-with-shade-loss-mitigation/