MIT developed batteries for ingestible medical devices. (Image Credit: MIT)
Swallowable devices have batteries with metals that aren’t safe for the body if the protective coatings wear out while moving through the digestive system. MIT researc...
The Olkiluoto site in Finland. (Kallerna/Wikimedia Commons)
A nuclear reactor, Olkiluoto 2, in Finland is expected to operate at 735 MW---155 MW below its full capacity until the end of next year. There were issues with its generator rotor that cau...
The Old Hickory Dam is being upgraded with a 7-blade turbine and new runners. (Image Credit: Mark Rankin/US Army Corps of Engineers)
Big projects usually don’t finish when first expected. At Tennessee’s Old Hickory Dam, ANDRITZ was suppo...
Agrovoltaics. (Image Credit: ADMC/pixabay)
For thousands of years, Egypt has made agriculture work in its harsh environment. Nowadays, however, farmers are facing more challenges: water scarcity and increasing temperatures that damage crops. Agrovo...
(Image Credit: Chandler Cruttenden/Unsplash)
Poor crabs. Aqueous zinc-metal batteries could be applicable for grid storage. After all, there is a lot of zinc, and it’s cheaper and safer than lithium. Conventional liquid electrolytes and polyme...
Artist’s concept of the Space Reactor-1 Freedom spacecraft flying past Mars. (Image Credit: NASA)
Solar power can be limited for deep space travel. When spacecraft move farther away from the sun, the sunlight reaching their solar panel weakens...
Diagram of the team’s research. (Image Credit: Kang et al., InfoMat 2026. Creative Commons Attribution License)
Fast charging cuts down on lithium-ion batteries charging time. However, transporting the lithium into electrodes at high rates le...
AI data centers use water to cool the servers. (Image Credit: UCR/Evan Fields)
I was wondering why water used in data centers can’t be reused. Nature cycles water constantly, it seems odd that the water is used to cool but then disappears. Why...
Figure showing the honeycomb-structured 3D PV design, the mechanical metamaterial support, and the light recapture mechanism. (Image Credit: Advanced Materials Technologies)
Although PV modules are useful, they have a flaw. They don’t retain a...
Roof tiles in the Villa of the Mysteries produce power. (Image Credit: Pompeii Archaeological Park)
Renewables in ancient cities?
While solar panels produce clean energy, there’s usually a catch. The problem? Solar panels affect the appearance...
(Image Credit: Wikimedia Commons)
MIT researchers recently created a new method to extract lithium from spodumene rock using a low-temperature process. A bathroom renovation inspired the research. At the time, Yet-Ming Chiang, MIT’s Kyocera Pr...
Comparing the neutral pH 7 with other battery technologies. (Image Credit: nature)
Researchers at the City University of Hong Kong have developed an aqueous battery with a pH 7 electrolyte. The battery system is built with water-based materials and ...
A solar farm. (Image Credit: TheOtherKev/pixabay)
Is that bad?
In the UAE, where water is harder to come by than oil, cloud seeding or desalination plants produce freshwater for everyone living there. Now, a 2024 modeling study says huge solar farms...
Deep Fission is a startup focusing on the burial of nuclear reactors as a cheaper, simpler alternative to traditional above-ground power plants. (Image Credit: Deep Fission)
Nuclear power is becoming more complex and costly, and one startup wants to...
Render and data show radiative cooling of the top plate to the night sky and warming of the bottom plate to the ground. This produced a temperature difference that powered the engine. (Image Credit: ScienceAdvances)
Engineers at the University ...
(Image Credit: Wikimedia Commons)
Wind and sunlight are the most common sources of renewable energy, powering turbines and solar panels worldwide. Japan and other countries are now tapping a subtler source: footsteps on piezoelectric sidewalks to ge...
Rendering of the co-firing hydrogen engine built by Kawasaki Heavy Industries. (Image Credit: Kawasaki)
Kawasaki Heavy Industries constructed the first-ever 8MW KG Series co-firing hydrogen engine, which generates electricity. It operates on natural...
Japan’s Chikyu deep-sea drilling vessel recently extracted samples of rare earth elements from seabed sediment. (Photo By Gleam - Photo taken by Gleam., CC BY-SA 3.0)
Japan is starting to take action on a decade-old plan to move away from Chi...
Hi Element14 Community!
Traditional alkaline batteries tend to "die" at the most inconvenient times. I used to I have them in devices like wireless mouse and keyboards, and it felt that the batteries were draining fairly quickly, catc...
Artist’s rendering of a lanthanide-doped nanoparticle in the shape of a spider and the web (made of 9-ACA). (Image Credit: Zhongzheng Yu/)
Engineers at the University of Cambridge have developed a technique that enables the electrical activati...
Unboxing the Multicomp Pro Professional Thermal Imager : A First Look
The fine (and clearly very patient) folks of the element14 Community somehow concluded that my particular brand of Halloween-themed tinkering deserved to win this year’s Hall...
(Image credit: Pixabay)
If you’ve ever designed a product meant to run off a battery and last a long time, you know how brutal reality can be. You start with hope and a 10,000 mAh battery, and six months later, you’re back in meeti...
The IE-TENG system generates electricity through the intrusion and extrusion of liquid in the silicon nanopores. (Image Credit: TU Hamburg, DESY, Künsting)
Engineers at Hamburg University of Technology (TUHH) and other European institutions dev...
Lonnie Johnson, inventor of the Super Soaker, is working on the JTEC device. (Image Credit: Johnson Energy Storage)
We’re familiar with the legendary Super Soaker, a fun water gun invented by Lonnie Johnson that earned him a $1 billion profit ...