Power & Energy
  • Technologies
  • More
Power & Energy
Blog OpEd: What India and Pittsburgh Have In Common
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 3 Jun 2017 3:00 PM Date Created
  • Views 1473 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

OpEd: What India and Pittsburgh Have In Common

rscasny
rscasny
3 Jun 2017

I think we all live with some level of tunnel vision. We live locally and too often are unaware of what is going on in the wider world despite our access to the reportage of world events.

 

I thought about my own tunnel vision of the wider world when I did my typical Saturday morning thing: got a cup of coffee from my local Starbucks and read in the New York Times the story: India, Once a Coal Goliath, Is Fast Turning Green.

 

The gist of the story is that India WAS planning on building a whole lot of coal-fired plants but are cancelling many of them because (a) their current plants are operating at only 60% capacity and (B) they are relying more on renewables such as solar power.

 

India, so says the story, is also decreasing its annual coal production from 660 million tons to 600 million tons -- down 10%.

 

Clearly, the world is embracing renewable energy technology. It appears to be making sense in India. It even makes sense to the mayor of Pittsburgh in the U.S. In another story, it says that  Pittsburgh already has 13,000 jobs in the renewable energy industry. Says the story, "Pittsburgh today is increasingly rebuilding around greener medical complexes, research university and tech offices." Less need for coal, for sure.

 

I haven't been to Pittsburgh since I worked for Eaton Corp. as a field engineer about 20 years ago. And I have yet to visit India. But this morning over a cup of coffee at my local Starbucks, my world view just got a wee bit bigger.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +4
    Interesting perspective, but there are other issues driving power in India. Agreed, they are reducing coal power, not so much to be Green, but because they do not have the power distribution infrastructure…
  • rscasny
    rscasny over 8 years ago in reply to DAB +2
    Don, I think you're right. Accompanying the story, was a picture of a solar panel on top of a man's home. Perhaps that's the only way from him to get power; the story didn't say. But India is indeed a…
  • rscasny
    rscasny over 8 years ago in reply to shabaz +2
    The inverters for appliances in RC (campers) in the US are fairly efficient and common so I shouldn't be surprised that solar cells can be used to feed them for appliance power and lighting in developing…
  • shabaz
    shabaz over 8 years ago in reply to rscasny

    Hi Randall.

     

    I agree, exactly that, the alternatives like generators have the major disadvantages of cost/maintenance (hardly anyone can afford them when they are earning $20 a week), also the villages are quiet generally (you can hear the other distant villages at night often). A generator is usually so loud it is impractical. Also, the cannisters of fuel (propane or similar I think) end up getting used in a domestic environment which to me feels unsafe, a few mm of rubber grommet sealing the hose is the distance between life and death : (

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago

    That was an interesting article. I see huge adoption of solar in villages in Pakistan, their main problem they are solving there is simply they cannot trust the mains supply, it regularly shuts down.

    The electricity companies 'round-robin' the supply to different towns/villages, so that everyone gets a time-slice of power for a few hours, because they don't have the capacity to power all of them simultaneously. It's not great : (

    The small solar cell provides a supply for running a couple of low-voltage (e.g. 12V) fans, and the stored energy can be used for running 12-volt LED lamps. Some will also have an inverter for running their fridges etc.

     

    Small solar panels and battery backup is commonplace there, although the cost is still high for people. Technically if we look at solar panels, the solar cells inside them are cheap, a lot of the cost is the waterproof and environment-proof structure.

    Taking solar cells and building them into solar panels could be an interesting project, especially if it can be done using easy-to-obtain materials. Another interesting project would be to develop efficient but high quality LED lighting for low-voltage

    use. A lot of the lighting I saw was awful, barely usable.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 8 years ago in reply to DAB

    Don,

     

    I think you're right. Accompanying the story, was a picture of a solar panel on top of a man's home.  Perhaps that's the only way from him to get power; the story didn't say. But India is indeed a big country. Surely the cost of running power to them is a lot. Perhaps this in another advantage of green power. Running a portable generator on fossil-type fuel would be another hill to climb for remote areas (costs, maintenance, etc.)

     

    Randall

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago

    Interesting perspective, but there are other issues driving power in India.

     

    Agreed, they are reducing coal power, not so much to be Green, but because they do not have the power distribution infrastructure to get the power from the generator to the people.

     

    India is BIG.  They have almost no way to effectively provide power to remote areas.  The cost to install a reliable power infrastructure is HUGE.

     

    Their solution is to go to local solar power.  Both due to the amount of sunlight most areas receive, but more importantly, it eliminates the cost and effort to create the distribution grid.

    In their situation local power is reliable, as long as the sun shines, requires minimal cost to install, and reduces the ravages of nature and theft.

     

    I applaud their engineering and management decision.  For them it makes very good sense to go local solar as they are starting at a very primitive level in most cases.

     

    Just my opinion.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<