Power & Energy
  • Technologies
  • More
Power & Energy
Forum What do you think of this E-Fuse Dev Kit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 283 subscribers
  • Views 1280 views
  • Users 0 members are here
  • e-fuse
  • st microelectronics
Related

What do you think of this E-Fuse Dev Kit

rscasny
rscasny over 6 years ago

eFuses, or electronic fuses, are integrated circuits that can replace larger conventional fuses or other protection devices such as resettable polymeric fuses. Housed in small plastic packages, such as DFN and Flip-chip, they integrate a control circuit and a power switch with low on-resistance, connecting the input port to the load.

 

When connected in series to the main power rail, an eFuse operates like a standard fuse with the ability of detecting and quickly reacting to overcurrent and overvoltage conditions. When an overload condition occurs, the device limits the output current to a safe value defined by the user. If the anomalous overload condition persists, the device goes into an open state, disconnecting the load from the power supply. The overload current limit can be programmed by means of an external resistor. An input overvoltage clamp function is available in the majority of ST's eFuses, therefore the load can also be protected against power supply regulation failure leading to input voltage excursion.

 

At turn-on, during power hot-plug or hot swapping of boards, the eFuse ramps up the output voltage in a linear and controlled way, which prevents a high inrush current flowing from the power source to the load, consequently avoiding power supply overload. This function is very useful in applications where a single power supply serves several loads connected to the same rail, such as HDD arrays and servers. The startup time is adjustable by changing a soft start capacitor.

 

The E-Fuse Dev Kitimage

The STEVAL-EFUSE01 allows full evaluation of the STEF01 E-fuse and is designed to help you test and develop a power path protection to the system. The STEF01 E-fuse integrates a control circuit and a low on-resistance MOSFET switch and provides a full set of protections, including overcurrent, overvoltage and inrush current. You can adjust UVLO threshold, clamping voltage and overload current limits through mechanical trimmers.

 

An external MOSFET, driven by the STEF01 gate driver pin, can be mounted to implement a reverse-current blocking circuit. The inrush current can be controlled by the output voltage ramp rate, with the dedicated soft start circuit embedded in the STEF01 device. The STEVAL-EFUSE01 evaluation board lets you easily adjust the output voltage ramp rate at the desired startup time, by changing the Cdv/dt capacitor.

 

As most applications require a flag to signal that the output voltage is in the correct range, the STEVAL-EFUSE01 features a PG test point for information about the voltage drop on the pass element. The STEVAL-EFUSE01 also features thermal latch and auto-retry thermal protection modes, selectable through a dedicated jumper configuration. For more informationFor more information

 

What Do You Think of This Kit?

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 6 years ago +2
    This is something I have been wanting to learn more about. I have an electronic load project that needs input protection from the DUT and the range of this device brackets it perfectly.
  • michaelkellett
    michaelkellett over 6 years ago +2
    It has pros and cons. The biggest con is that it is incomplete, offering no reverse voltage, spike or load reverse current protection - all these things are commonly required and the justification for…
  • dougw
    dougw over 6 years ago

    Neat device.

    I am currently toying with building an application that needs a fuse, however I wasn't planning on having 8 V available to run a device like this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago

    This is something I have been wanting to learn more about.  I have an electronic load project that needs input protection from the DUT and the range of this device brackets it perfectly.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neuromodulator
    neuromodulator over 6 years ago

    Note that eFUSEs are something completely different

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 6 years ago

    So is this relatively new? I noticed the revision date was in May 2019. Looks interesting at this point. Wonder if a Road test is around the corner. Hint hint rscasny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago

    It has pros and cons. The biggest con is that it is incomplete, offering no reverse voltage, spike or load reverse current protection - all these things are commonly required and the justification for using a complex device rather than a nice simple fuse or polyfuse would be that you got all the goodies in one package.

    Additionally the current trip is not well specced (how fast is it ?) , not accurate and not sufficiently adjustable (no time to respond control).

     

    There will be applications where this chip is a good fit and many where it is not - it is quite cheap.

     

    One big show stopping question is  - does it fail open or short circuit ?

    Wire fuses, and to a lesser extent polyfuses are very predictable in this respect.

    Do I trust a complex device where failure  = fire ?

     

    As ever with Dev kits - you only really learn if part is any good to you when it's on your own board, sometimes a dev kit will tell you it's not worth doing a board. This kit has the virtue of being simple and cheap !

     

    MK