Power & Energy
  • Technologies
  • More
Power & Energy
Forum 12V Low Battery Cutoff
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 284 subscribers
  • Views 6912 views
  • Users 0 members are here
Related

12V Low Battery Cutoff

logiclevel14
logiclevel14 over 6 years ago

I am looking for the best/lowest current draw way to create a low battery cutoff for a 12v battery powered circuit.  The battery will power a micro-controller and also a number of solenoids that may draw up to 10 amps.  Because of the high amperage draw lithium ion batteries may be out of the question.  I could be wrong but when dealing with a high amperage draw, a NiMh may be the better solution.  The amperage will draw be of a short duration, probably 1 second.  I know it is common for lithium ion batteries to have built in low battery cutoff circuits but when dealing with a standalone NIMh battery or any other generic 12v battery what would be the best way to set up a low battery(10.6v) cutoff?  There are low battery cutoff modules, but I find these to be defective half the time and they draw too much current.  There are low battery cutoff IC's I see but they only deal with low voltage supplies like 5v or less.  Does anyone know of a low voltage cutoff ic that works with 12v batteries?  I may or may not be using a 555 timer and/or an attiny85 microcontroller in the circuit.  Can these devices be used to create a low voltage cutoff?  I programmed an arduino to cutoff the voltage at 10.5 volts using the serial monitor but I could only get this to work when the Arduino was plugged in to computer via usb.  Does serial monitor work with a microcontroller when powered by battery alone or does it need to be plugged into a computer via usb?

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 6 years ago +7
    Here is a device that sounds like what you are looking for: http://www.ti.com/lit/ds/symlink/tl7702a.pdf . The TL7712 device is a 12 volt monitor that trips if the voltage drops below 10.8V. Current draw…
  • shabaz
    shabaz over 6 years ago +3
    This is really hard to follow. There's a lot of assumptions here, so in-between those assumptions I'm not confident in the 'probably 1 second' and 10 amps values too. Could you supply a circuit diagram…
  • logiclevel14
    logiclevel14 over 6 years ago in reply to genebren +3
    Thank you gene I think this should do it.
Parents
  • shabaz
    shabaz over 6 years ago

    This is really hard to follow.

    There's a lot of assumptions here, so in-between those assumptions I'm not confident in the 'probably 1 second' and 10 amps values too. Could you supply a circuit diagram of what you're thinking of, and the part codes, and what the aim of the circuit is?

    Any circuits or project links you're following, to help progress your project, or is this some completely unique project and you're starting from scratch (not a good idea for a project involving the combination of items you mention).

    All this detail is needed because the answers could change significantly depending on that information.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to shabaz

    Another satisfied customer. Create an account and in less than 12 hours you get an answer.

     

    Maybe it will produce and active member?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to colporteur

    Is that a question to me?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • logiclevel14
    logiclevel14 over 6 years ago in reply to colporteur

    are we hurting for active members?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to logiclevel14

    Yes, the community is always looking for new members. Active would be members willing to  contribute as wells satisfying there own needs. Active members are most welcomed.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 6 years ago in reply to logiclevel14

    Yes, the community is always looking for new members. Active would be members willing to  contribute as wells satisfying there own needs. Active members are most welcomed.

    • Cancel
    • Vote Up +3 Vote Down