Power & Energy
  • Technologies
  • More
Power & Energy
Forum Regulated Power Supply for LED Spot Light
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 286 subscribers
  • Views 1435 views
  • Users 0 members are here
Related

Regulated Power Supply for LED Spot Light

bheemarao
bheemarao over 15 years ago

Hi

 

My requirement is Power supply for LED Spot light.

 

i want to drive 5 High power LED  18V @ 700mA so i am into design of power supply and the component should be easily available.

 

can any one suggest me the solution

 

Best Rgds

Bheema

  • Sign in to reply
  • Cancel
Parents
  • bheemarao
    bheemarao over 15 years ago

    Hi,image

     

    i had done the below circuit and tested, it is working fine but the maximum current deliver in only 200mA max, can any one suggest me the solution for driving 1A.

     

    Best Rgds

    Bheema

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenW
    WarrenW over 15 years ago in reply to bheemarao

    Looking at the design, it seems this is most likely drive from main voltages and therefore quite likely to be a 50 or 60 Hz supply. In this case the capacitor you have choosen as you filter (1uF C3) is way too small. Try increasing it to 1000uF. As a general rule of thumb I use 1000uF per Amper per volt drop as a guidline. e.g 1000uF filter @ 1 A load should equate to approx 1 volts drop in the supply volts to the regulator. You have shown a 1uF filter capacitor (C3) so virtually no regulation exists before the LM350 and I would expect in those circumstances to see quite an AC component on your 'regulated' DC output.

     

    Cheers

     

    Warren.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • WarrenW
    WarrenW over 15 years ago in reply to bheemarao

    Looking at the design, it seems this is most likely drive from main voltages and therefore quite likely to be a 50 or 60 Hz supply. In this case the capacitor you have choosen as you filter (1uF C3) is way too small. Try increasing it to 1000uF. As a general rule of thumb I use 1000uF per Amper per volt drop as a guidline. e.g 1000uF filter @ 1 A load should equate to approx 1 volts drop in the supply volts to the regulator. You have shown a 1uF filter capacitor (C3) so virtually no regulation exists before the LM350 and I would expect in those circumstances to see quite an AC component on your 'regulated' DC output.

     

    Cheers

     

    Warren.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • bheemarao
    bheemarao over 15 years ago in reply to WarrenW

    Thanks Warren,

     

    I will try changing C3 to 1000uf.

     

     

    Best Rdgs

    Bheema