Power & Energy
  • Technologies
  • More
Power & Energy
Forum Free energy?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 288 subscribers
  • Views 4127 views
  • Users 0 members are here
Related

Free energy?

enrico.migchels
enrico.migchels over 16 years ago

Hi there,

 

There are several posts on the Internet from people who claim to have found the energy 'holy grail'. Meaning machines which convert energy from one form the another without loss or even with energy gain. What do we do which such claims as there is no one who has produced a machine that is in normal use somewhere by someone.

 

Personally i am strong non-believer of free energy devices, as they seem to contradict the law's of physicsas as we know them.

 

Please share your idea's and comments on this topic.

 

Best regards,

 

Enrico Migchels

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 14 years ago in reply to FredM +2
    Personally, I find that sanity is just social concensus. 6443.contentimage_938.png I am amazed at the number of people that think we have an energy shortage. From my analysis, we are using just a small…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi, -This is my first topic so I hope I won't make mistake. I strongly agree with you, but sometime it's possible to "harvest" a small quantity of energy that can be used to produce energy. For example…
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor +1
    Hey, new to this, but very interested in converting heat to electricity! Can you explain the theory behind a pelcier cell? I'm having a little trouble finding anyone to explain it to me, it seems like…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    don't need, ask the goverment for ur solar panel support, then pay some

    for yourself, few years later, you get true free energy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    don't need, ask the goverment for ur solar panel support, then pay some

    for yourself, few years later, you get true free energy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    With this kind of "application" it's very important the "insurance": inverters are very fragile and after few years can broken. If you have some problems and you have to change some pannels you may not be able to install the same kind (ame voltage and current) of pannel: so the performance of you system can become very low due to the "incompatibility" of the new pannels. For example: you have a system of 7 pannels and if, after 10 years, you have to change a pannel moving from In=10A to In=5A, all the system can erogate 5A at maximum...
    If you have to change the inverter you have to wait for the new one: In "my" system I had to wait for a month... so the system was down for a month and it was not able to produce energy and money.
    I call that "TRUE LIFE"...
    And, as last... WE pay the goverment: so WE pay for solar energy... I'm not sure we can call the Solar energy as "free energy".
    I think that solar energy it's usefull only with small and distribuite applications.

    With this kind of "application" it's very important the "insurance": inverters are very fragile and after few years can broken. If you have some problems and you have to change some pannels you may not be able to install the same kind (ame voltage and current) of pannel: so the performance of you system can become very low due to the "incompatibility" of the new pannels. For example: you have a system of 7 pannels and if, after 10 years, you have to change a pannel moving from In=10A to In=5A, all the system can erogate 5A at maximum...

    If you have to change the inverter you have to wait for the new one: In "my" system I had to wait for a month... so the system was down for a month and it was not able to produce energy and money.

     

    I call that "TRUE LIFE"...

     

    And, as last... WE pay the goverment: so WE pay for solar energy... I'm not sure we can call the Solar energy as "free energy".

     

    I think that solar energy it's usefull only with small and distribuite applications.