Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar Panel, Self Build
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 282 subscribers
  • Views 293 views
  • Users 0 members are here
Related

Solar Panel, Self Build

enrico.migchels
enrico.migchels over 15 years ago

Hi there,

 

I bought a stack of PV cells on e-bay. The idea is to experiment with solar power and to get knowledge of transferring energy from the cells to a load (battery, grid) with the highest efficiency possible. The specification of the PC cells are really nice (8.88A / 4.35W per unit, 15 x 15 cm. The problem I am facing now is that the cells are really fragile (silicon plate, 200micron thickness). After soldering copper strips (100micron) on the pre-tinned cells,  the cells are not completely flat due to the thermal expansion during soldering. I guess this is bad for the lifetime. Mounting the cell on a backplate will be done with 1 dot of glue in the middle to avoid further thermal expansion stress on the cells.

 

Has anyone experencie with self-build solar panels? Or does anyone know about websites describes this?

Also, I do not often see a mechanical sun tracker on solar systems. Is this too complicated to make or is the extra generated energy too small compared to the investment?

 

Best regards,

 

Enrico Migchels