Power & Energy
  • Technologies
  • More
Power & Energy
Forum LED Street Lighting Power supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 284 subscribers
  • Views 6312 views
  • Users 0 members are here
  • driver
  • lighting
  • led
  • supply
  • street
  • power
Related

LED Street Lighting Power supply

Jason
Jason over 16 years ago

Hello All,

As we know, LED is used moreand more on street lighting, in the future, LED will replace the traditional street lighting bulb. Many supplier have there own power supply solution for LED street lighting, such as NXP, ON, PI,TI, Fairchild and so on, some solution is isolated Fly-back and some is non-isolated high voltage Buck to drive LED bulb, some solution use PFC controller and some use Valley PFC circuit to increase power factor. The question is which solution is more popular for the LED street lighting? isolated or non-isolated,  PFC controller or Valley PFC circuit?

  • Sign in to reply
  • Cancel
Parents
  • Jorge_Garcia
    Jorge_Garcia over 16 years ago

    Hi Jason,

     

    Hope you are doing well.

     

    I agree with Enrico in that you are better off using an active PFC based off a boost converter. The performance of the Valley Circuit is not going to be good enough for Street Lighting. However, I disagree with his recommendation of using an LLC resonant converter. The resonant converter topology is very common for Fluorescent Ballasts and the like however there's no need to go with such a sofisticated topology to drive LEDs.

     

    An active PFC gives a 400V rail, a well designed buck topology could be used to power the LEDs. The simplified conversion function for a buck controller is Vo=D*Vin the current relationship similarly is In=D*Io, I bring this up because even though the PFC stage stepped up the voltage the current you'll be able to draw from it won't be very great depending the Power output you have designed for. The buck topology takes in very little current for a given output current depending on the conversion ratio so it meshes very well with the PFC stage.

     

    I've designed drivers that make use of both the Buck and Boost topologies and they are simple to implement in an LED design. As Enrico mentioned these topologies are not isolated so if for safety reasons you must use an isolated supply then you may have to use one of the isolated topologies such as a Flyback. I mean no disrespect to Enrico his solution is valid, I just think it's more complicated then it needs to be.

     

    hth,

     

    Best Regards,

     

    Jorge Garcia

    Cadsoft Computer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 16 years ago in reply to Jorge_Garcia

    Hi Jason,

     

    Ok, probably the active PFC and flyback is better . I have found an interesting article:

     

    http://powerelectronics.com/power_management/lighting_power_management/led-streetlight-high-brightness-0225/

     

    Jorge, we use LLC all the time :-) We like the EMI behaviour and the lack of stress on the power components. :-) Okay, you are the expert! ;-)

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 16 years ago in reply to enrico.migchels

    According to Element-14 standings you're the expert. image

     

    Jason,

     

    I'm sure Enrico will agree with me that we hope our responses have proven to be helpful in giving you some guidance as to how to proceed with your LED streetlight project.

     

    Here to help,

     

    Jorge Garcia

    Cadsoft Computer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jason
    Jason over 16 years ago in reply to Jorge_Garcia

    Hi Enrico, hi Jorge,

     

    Thanks for your responses! It is very useful to my project.

     

    I have designed a 350W LCD TV(52 inch)  power supply which use a active PFC and a LLC. I have to say that PFC+LLC is good choice for power supply >200W.  But this LED Street project only 36W, use active PFC+LLC will increase my cost. What about the Single-Stage Flyback topology which use PFC IC as its PWM controller? This solution can match both the PF requirement and safety requirement. The architecture as bellow:image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 16 years ago in reply to Jason

    Hi Jason,

     

    By looking at your diagram, even if you are using a PFC chip to control the Flyback stage that doesn't mean you get built-in power factor correction. The only feedback loop your showing in the diagram is the LED current control loop. As you know in order to implement a PFC control algorithm you would have to monitor the input voltage waveform and inductor current.

     

    If the biggest issue is price, then you may want to consider passive power factor correction. Granted I hope you don't have any size restrictions because the inductor you're going to need to implement passive power factor correction will be fairly large. This solution will work well as long as the number of LEDs you plan to drive is going to be constant, passive power factor correction tends to work best when you have a fixed predictable load.

     

    Using a Passive PFC circuit will improve power factor to about .75-.85. If I remember correctly the latest energystar guidelines specify that devices consuming less than 75W must have a power factor of .7 or better. If I'm wrong I'm sure someone will correct me, but this could be an option since your driver is only for 36W.

     

    I believe that your solution of a single stage-flyback+Active PFC should be lower in cost than LLC+Active PFC.

     

    hth, and if I made a mistake in any of my statements please someone correct me.

     

    Regards,


    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jason
    Jason over 16 years ago in reply to Jorge_Garcia

    Dear Jorge,

     

    Brilliant analyse.

     

    I'm sorry I don't show all the feedback loop that make you confused, there have other loop from the output of the bridge-rectifier and inductor current.

     

    Generally, >75W power supply require PF>0.9, but for LED application, Commercial ≥ 0.90, no matter how many watt of the power supply,you can find the requirements by the following link:

    ENERGY STAR Requirements for SSL Luminaires, Version 1.1 (page4 Residential ≥ 0.70 Commercial ≥ 0.90)

    http://apps1.eere.energy.gov/buildings/publications/pdfs/ssl/energystar_sslcriteria.pdf

     

    And, you can also find a Single Stage PFC solution of power supply in ON-Semi's website:

    A Single Stage PFC+PWM Converter for 75-150 W Distributed Power

    http://www.onsemi.com/site/pdf/ipecsa_paper.pdf

     

    Maybe this solution is suitable for my application.

     

    Do you have any idears?

     

    Best Regards

     

    Jason

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 16 years ago in reply to Jason

    Hi Jason,

     

    It looks feasible, obviously you would have to modify the Feedback loop to regulate current instead of the output voltage (the tested design is set to output 12V).

     

    The only point of concern is what input line voltages you plan to use your driver at. If you notice on the charts of page 5 the power factor falls below 0.9 at high line voltage and low output power. I looked at the standard and it doesn't specify at what conditions that power factor must be greater than 0.9. From this we can deduce that the power factor must be greater than 0.9 for all operating conditions, if that's the case then under some circumstances the App Note design will not meet the specifications.

     

    If you plan to design the driver for a specific line voltage then you could optimize it for that specific line voltage, if not you will have to look at another solution.

     

    Your designing a low power driver (36W), TI and National semiconductor have some good chips that you may be able to use. I know National doesn't make a PFC chip (other than their triac dimmable driver) but TI makes a couple. You may be able to then use one of National's specifically designed drivers, for the driver stage.

     

    Check out TI's LEDCookbook.

     

    http://focus.ti.com/lit/sg/slyt349a/slyt349a.pdf

     

    You should find pages 10-18 very interesting

     

    hth,

     

    Best Regards

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Jorge_Garcia
    Isolated drivers are typically implemented because they simplify and improve the LED module/array connection to the heatsink. Typically Street lights have a good amount of external surface that can help the heatsinking strategy so isolating it the LED driver from the LEDs allows one to take better advantage of thermally connecting the LED array to the external surface. Also, typically street light certification requires some level ingress protection (IPxx) and general UL safety. Isolating the LED array from the AC input helps with that requirement as well.
    Active PFC control is better because it is more efficient that Valley fill PFC. Valley Fill PFC is ok low power lighting applications – like residential - but the extra dissipation usually does not make it favorable to higher power applications like street lighting.
     
    TI has soem veru cost effective Street lighting LED driver solutions that will cost effectively help with the requirements and issues mentioned in this discussion.
     
    http://focus.ti.com/general/docs/gencontent.tsp?contentId=28887
     
    I hope this helps.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 16 years ago in reply to e14 Contributor

    Hi Guys,

     

    A lot is being said about topology choices and implementations. Enough to build something worthwile. Anyway, i like to share some interesting; the near future of power control.

     

    AN1271 : Isolated Flyback converter to drive LEDS with active PFC function.

     

    http://ww1.microchip.com/downloads/en/AppNotes/01271A.pdf

     

    The scheme is not fully digital control as the microcontroller has analog peripherals for the control loop. This is a very nice way to make the next step. I have samples on my desk of this controller, now i have to find the time to play with the device.

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • firatkocak
    firatkocak over 16 years ago in reply to enrico.migchels

    Hi Enrico,

     

    Great document! I think i am trying to build that circuit int the next days to see how it works. And i would be glad to hear about your experiments though.

     

    Thanks for your sharing.

     

    Firat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jason
    Jason over 16 years ago in reply to Jorge_Garcia

    Hi Jorge,

    I will set three type of output current beforehand which is 350mA, 700mA, 1050mA, that means my full load is about 36W and my light load is only 12W. The power factor become the big problem when light load and high voltage input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jason
    Jason over 16 years ago in reply to e14 Contributor

    Hi Peter,

    Lighting certification and safety requirement is the main reason to design a Isolated driver, but the cost also take into account, maybe the Single-Stage Flyback is the best choice. What you say?

     

    Jason

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jason
    Jason over 16 years ago in reply to e14 Contributor

    Hi Peter,

    Lighting certification and safety requirement is the main reason to design a Isolated driver, but the cost also take into account, maybe the Single-Stage Flyback is the best choice. What you say?

     

    Jason