Power & Energy
  • Technologies
  • More
Power & Energy
Forum Free Grid-Connected Digital Power Reference Design for Solar Panels
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 283 subscribers
  • Views 821 views
  • Users 0 members are here
  • microchip
  • reference
  • Design
  • inverter
  • grid-connected
  • panel
  • solar
Related

Free Grid-Connected Digital Power Reference Design for Solar Panels

GardenState
GardenState over 15 years ago
Solar design engineers are being challenged to optimize energy harvesting, reduce installation costs, and improve system reliability and efficiency while standardizing their designs.

Microchip today announced a digitally controlled, grid-connected solar micro inverter reference design. The reference design connects to any standard solar panel and converts the panel’s DC output into AC power, which can then be fed into the public power grid. In a real-world application, multiple units can be connected together to achieve the desired power output.

This reference design works with any photovoltaic (PV) panel that supplies a maximum 220 watts output, and it comes in two versions supporting either 110V or 220V power grids. Both versions of this reference design are implemented using a single dsPIC33F ‘GS’ digital-power digital signal controller (DSC), which provides digital control of the power-conversion and system-management functions.
 

Complete documentation, including software, schematics and application note, can be downloaded for free by clicking here.

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    enrico.migchels over 15 years ago

    Hi Garden State,

     

    Thanks, this post is spot-on! Any new development in the field of renewable energy draws my attention. It also proves that it is worthwhile to keep touch with the technical community on element-14. Now let's see if Microchip is willing to send this application to play with :-)

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • enrico.migchels
    enrico.migchels over 15 years ago

    Hi Garden State,

     

    Thanks, this post is spot-on! Any new development in the field of renewable energy draws my attention. It also proves that it is worthwhile to keep touch with the technical community on element-14. Now let's see if Microchip is willing to send this application to play with :-)

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • awinning
    awinning over 15 years ago in reply to enrico.migchels

    Hey Enrico

     

    Is it not all there for download free?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 15 years ago in reply to awinning

    Hi Ali,

     

    I know that Microchip makes a number of reference design board for customers to review and test. The number is always limited because of the value of these boards, it can mean that you have to wait until it is your turn to play with the board. If you think you can speed up things, feel free to help out.

     

    I have reviewed the Digital AC/DC power supply design reference board already and I was impressed. This stuff is really interesting and worthwhile to review on Element-14 also.

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to enrico.migchels

    Enrico,

     

    I can't promise you anything, but I'll have a go for you. Sounds like a really good product to test.

     

    Ally