Power & Energy
  • Technologies
  • More
Power & Energy
Forum Should i try using an ultracap?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 283 subscribers
  • Views 1209 views
  • Users 0 members are here
  • dc-dc
  • alternative_energy
  • power_management
  • ultracap
  • power_supply
  • ultracapacitor
Related

Should i try using an ultracap?

e14 Contributor
e14 Contributor over 15 years ago

Im currently having the pleasure of working on a project where the cost of components is of little importance.

It's fun to work in this new way, but i find myself having trouble choosing components now that "the entire market is open to me"..

 

Here's the setup:

 

I'm designing a product that is to be powered by a regular switchmode DC supply. Minimum is 12Volts and 1 ampere (actually closer to 600mA)

 

The thing that's tricky is that the product has to retain it's power for 30 seconds after removal of the DC supply.

 

Meaning that i need a battery or supercapacitor that can supply at minimum 12V @ 600mA for 30 seconds.

 

I've already found a LiPo battery that can supply this. But am missing several key points in this particular design (charge circuit, power source chooser, step-up conversion to 12V and so on)

 

It would be so much easier if i could just put a super-cap in parallel with the supply, and let that take care of the 30 seconds of extra power, but i have no idea how to dimension a supercapacitor.

and, quite frankly, they scare me...

 

Any suggestions?

 

Regards

-Mark

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    enrico.migchels over 15 years ago

    Hi Mark,

     

    Difficult problem. This is what I would try/do.

     

    Energy storage on the low voltage output of the power supply is difficult. You need to have a very large tank (a battery would do that) but if you want to run the application from a capacitor you have serious problems. You talk about 12V / 600mA / 30seconds. That is 216J. A really large amount of energy. Probably your application is sensitive for voltage drops, so a discharging 12V capacitor (12V will decrease slowly) will cut out the application before the capacitor is drained.

     

    You can try the following. Buy a power supply with an PFC circuit in. This is an input voltage booster which charges the primary elcap to 400V, independent from the input voltage. This circuit is standard incorporated in 75W+ power supplies. Storing electrical energy on the primary side is in your case 1000 times more efficient and... the power supply does not mind that the 400V capacitor is discharging slowly under mains voltage removal. The primary controller adjusts its regulation setpoint to keep the output voltage steady on 12Vdc. You can add extra capacitance on the 400Vdc bus if desired. Additional you should examine if your application should run with 100% functionality or if it is allowed to switch off certain circuits (to lower the 600mA consumption). You can easily make a mains dip detection circuit on the secondary side of the power supply. This can act as a signal to switch off certain circuits.

     

    For example: in LCD-TV's the backlighting is cut-out in case of mains dips, this is 100W less load... It can be substantial.

     

    Maybe this can help you.

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to enrico.migchels

    A PFC smps! of course! that's brilliant!

     

    Thank you for your help!

     

    any advice on which one to buy? ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 15 years ago in reply to e14 Contributor

    Hi Mark,

     

    Buying a SMPS with PFC circuit alone won't be enough. You have to tweak both the application and the smps.

     

    If you need 12V @ 0.6A for 30s this means 216J (240J transferred to the primary input of the smps, efficiency 90%)

     

    If the smps is able to be in regulation at 100VDC this means that the capacitor voltage is allowed to drop from 400V to 100V in 30s with a constant load of 8W. This would mean that you need a PFC elcap of about 5mF. This is a very big and expensive device :-)

     

    If you detect mains failure with an opto-isolator (very simple circuit) and you can cut-out a large portion of the load the value of the PFC elcap comes down.

     

    For example: load consumption in mains failure mode 100mA. This would mean 1.3W input power. The capacitor value comes down to 800uF. And so on.

     

    I would say: focus on the application first and then.. focus on the SMPS.

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to enrico.migchels

    I've talked to my employer, and we've bargained back and forth. when he realized how expensive this setup would be he allowed me to go down to 10 seconds instead of 30.. the 600mA is a bare minimum i'm afraid. But this still reduces the Joules needed by 2/3, so i'm quite pleased with this. what do you think? .. can it be done?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    For the PFC solution, you need to add substantially to the primary storage capacitor value. This will of course, mean that it no longer operates in PFC mode, as it is charging the caps to full voltage all of the time i.e. the charge current will not be sinusoidal. A battery really IS the way to go. 'Supercaps' are going to present a voltage that falls immediately once power is removed.

     

    I agree with Enrico here - you really have to tailor the application to be as 'backup friendly' as possible before trying to power it. You also realise that a $65 UPS in front of the PSU will do all of this, if you send it a shutdown signal after 10-30 seconds?

     

    I hate 'cost is no object' projects, because if you cannot satisfy the client's bizarre requirements, it reflects upon one's abilities as an engineer. Many times it is simpler to say "no, it cannot be done". In your case, it's more a matter of "you should have thought about this before you tried to get me to bypass any semblance of common-sense and try to break the laws of physics"!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    For the PFC solution, you need to add substantially to the primary storage capacitor value. This will of course, mean that it no longer operates in PFC mode, as it is charging the caps to full voltage all of the time i.e. the charge current will not be sinusoidal. A battery really IS the way to go. 'Supercaps' are going to present a voltage that falls immediately once power is removed.

     

    I agree with Enrico here - you really have to tailor the application to be as 'backup friendly' as possible before trying to power it. You also realise that a $65 UPS in front of the PSU will do all of this, if you send it a shutdown signal after 10-30 seconds?

     

    I hate 'cost is no object' projects, because if you cannot satisfy the client's bizarre requirements, it reflects upon one's abilities as an engineer. Many times it is simpler to say "no, it cannot be done". In your case, it's more a matter of "you should have thought about this before you tried to get me to bypass any semblance of common-sense and try to break the laws of physics"!