Power & Energy
  • Technologies
  • More
Power & Energy
Forum High power, high speed switching into resistive (heating element) load
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 563 views
  • Users 0 members are here
  • alternative_energy
  • Design
  • power
Related

High power, high speed switching into resistive (heating element) load

e14 Contributor
e14 Contributor over 15 years ago

Hello,

     can someone guide me on the best or simplest way to control the power supplied to a heating element(s).

     Power in range up to 10kW, voltage AC to 300VAC or rectified to DC.

I was thinking of using an IGBT module or a power Mosfet module and controlling with a PWM signal with a frequency of 10-20kHz.

Will this work, any and all assistance welcome please.

  • Sign in to reply
  • Cancel
Parents
  • Malcolm
    Malcolm over 15 years ago

    How about Farnell part number 1305681 ? RELAY, SOLID STATE, PA, 50A/230V http://uk.farnell.com/celduc/so445420/relay-solid-state-pa-50a-230v/dp/1305681 This is a phase angle controller (will generate quiet a bit on electrical noise, EMI), ideally a Burst fire comtroller would be better (zero cross over) but cannot see one. You control the heating using a Analog Input : 4-20mA. Regards Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Malcolm
    Malcolm over 15 years ago

    How about Farnell part number 1305681 ? RELAY, SOLID STATE, PA, 50A/230V http://uk.farnell.com/celduc/so445420/relay-solid-state-pa-50a-230v/dp/1305681 This is a phase angle controller (will generate quiet a bit on electrical noise, EMI), ideally a Burst fire comtroller would be better (zero cross over) but cannot see one. You control the heating using a Analog Input : 4-20mA. Regards Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Malcolm

    Any more suggestions please.