Power & Energy
  • Technologies
  • More
Power & Energy
Forum Lithium-ion charging schemes, or modules?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 283 subscribers
  • Views 1701 views
  • Users 0 members are here
  • dc-dc
  • management
  • controller
  • power_management
  • lithium_ion
  • Design
  • battery
  • Technology
  • power_supply
  • power_conversion
  • power
  • power.power
Related

Lithium-ion charging schemes, or modules?

Eavesdropper
Eavesdropper over 15 years ago
For an ongoing project of mine, I want to add energy storage to the system. I would like to use lithium-ion batteries for now, due to the joule density and price. However, I have never designed a charger for lithium-ion, or any battery for that matter, and need some guidance.
 
 
What are some schemes for charging?
Off the shelf products that I could just drop into a system?
Or links to some resources on the subject?
 
 
Some background on the project. I have an intermittent supply. I want to be able to charge the battery and run a load off the supply or battery at the same time.
 
 
Any help would be appreciated.
 
 
E
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Lithium-Ion is charged with scheme known as CCCV(i.e Constant Current Constant Voltage).Since the impedance of the battery is very low always it is required to control the current else it will cause gasing and result can be dangerous.

     

    For your application there are many standard IC's available from TI,National,Maxim,Intersil etc.

     

    http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?&familyAliasId=1000411&familyId=411&uiTemplateId=NODE_STRY_PGE_T&techFamId=null&rootFamilyId=null&sectionId=null&tabId=null&appId=null&viewDeviceCallingPage=null&totalCount=262&showAdditionalParameters=no&lc=3000435&lc=3000430&lc=3000431&lc=3000432&lc=2001192&compare=yes&download=yes&sort=yes&customize=yes&paramResults=yes&paramCriteria=yes&familyTree=yes&military=no&baSystem=yes&paramTable=no&sortOption=PA_PARAMETER_2001636&sortMode=DESC&searchPaths=1000394&pageId=undefined&templateId=0&navigationId=0&family=analog&paramTable=no&military=no&compare=yes&download=yes&sort=yes&customize=yes&paramResults=yes&paramCriteria=yes&familyTree=yes&military=no&baSystem=yes&paramTable=no&sortOption=PA_PARAMETER_2001636&sortMode=DESC&searchPaths=1000394&pageId=undefined&uiTemplateId=NODE_STRY_PGE_T&techFamId=null&rootFamilyId=null&sectionId=null&tabId=null&appId=null&viewDeviceCallingPage=null

     

    http://para.maxim-ic.com/en/search.mvp?fam=batt_chrg&tree=powersupplies

     

    http://www.maxim-ic.com/appnotes10.cfm/ac_pk/5

     

    Choosing a Li-ION battery charger is based on the efficieny requirement of your system.Thee are two types Linear and Switched.First one is less efficient but component count is less(also cost) and the 2nd one would be highly efficient(and cost image).

     

    Also it is important to add a hysterysis at the switch which controls the supply switch over.

     

    Regards,

    Arun

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to e14 Contributor

    Arun,

     

    Welcome to Element 14. Thanks for the reply. It is in depth.

     

    On the hysterysis point, any thoughts on how to implement a solution? I was thinking of adding a supercapacitor bank to rapidly store energy, and form there charge the batteries for longer term storage.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Eavesdropper

    Eves,

     

    I hope post by heath gives you a good understanding of the system and also about implementing the Hysterysis part.You can implement it using a widow(or a hysterysis) comparator or discrete circuitry based on transistors.But the discrete will not be a good solution since the switching between the supplies may not be ideal.

     

    I agree using the super capacitor bank will yield a better charge capacity and extends the longetivity of the battery.I feel using a supercapacitor bank shall be quite costly because of the protection required to be provided(like inrush current limit).There are many standard products(Li-Ion chargers and battery gauges) which can make your system look less costly.

     

    I am not sure if i understood your question correctly.Let me know.

     

    Regards,

    Arun

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Eavesdropper

    Eves,

     

    I hope post by heath gives you a good understanding of the system and also about implementing the Hysterysis part.You can implement it using a widow(or a hysterysis) comparator or discrete circuitry based on transistors.But the discrete will not be a good solution since the switching between the supplies may not be ideal.

     

    I agree using the super capacitor bank will yield a better charge capacity and extends the longetivity of the battery.I feel using a supercapacitor bank shall be quite costly because of the protection required to be provided(like inrush current limit).There are many standard products(Li-Ion chargers and battery gauges) which can make your system look less costly.

     

    I am not sure if i understood your question correctly.Let me know.

     

    Regards,

    Arun