Power & Energy
  • Technologies
  • More
Power & Energy
Forum High-reliability DC/DC Converter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 283 subscribers
  • Views 347 views
  • Users 0 members are here
Related

High-reliability DC/DC Converter

www.bestcetc.com
www.bestcetc.com over 15 years ago

Mil/COTS  hybrid thick film HQX28 series high-reliability DC/DC converter can work at specified input voltage, the max. output power is 216W and efficiency is as high as 90%.Mil-grade hybrid HQX28 series high-reliability DC/DC converter adopts push-pull topology technology, and the constant switching frequency is 80~120kHz.

Mil/COTS  hybrid thick film HQX28 series high-reliability DC/DC converter is made by the thick-film hybrid integration process and is totally sealed in a metal package. Both the design and manufacture of the Mil/COTS  hybrid thick film HQX28 series high-reliability DC/DC converter satisfy the requirements of GJB2438A-2002 “General specification for packages of hybrid integrated circuits” and specific specification of the product. The input end turn on the HMD-CE03F power filter, can be improvement the electromagnetic compatibility performance for Mil/COTS  hybrid thick film HQX28 series high-reliability DC/DC converter .

The features of the Mil/COTS  hybrid thick film HQX28 series high-reliability DC/DC converter

Range of input DC voltage: 24~32V, nominal input DC voltage 28V

Output power: 216W

Operating temperature (Tc): -55~+125℃

Input, output and package are isolated mutually

Insulation resistance: R≥100MΩ(DC 500V)

Efficiency reaches as high as 90%

Totally sealed metal package

E-commerce:www.bestcetc.com

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Saying thanks will not just be enough, for the extraordinary lucidity in your writing. I will immediately grab your rss feed to stay privy of any updates

     

    http://xn--4dbdjaba1aawcpi1a0c8cub.com
    tooth whitening pen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Saying thanks will not just be enough, for the extraordinary lucidity in your writing. I will immediately grab your rss feed to stay privy of any updates

     

    http://xn--4dbdjaba1aawcpi1a0c8cub.com
    tooth whitening pen