Power & Energy
  • Technologies
  • More
Power & Energy
Forum Inflatable wind turbine
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 283 subscribers
  • Views 522 views
  • Users 0 members are here
  • research
  • alternative_energy
  • energy_harvast
  • alternative
  • renewable
  • power
  • innovation
Related

Inflatable wind turbine

Eavesdropper
Eavesdropper over 14 years ago
image
Dean Kamen's Inflatable Wind Turbine, via the USPTO
 
There may be a new idea on the rise that is not full of hot air. Inventor Dean Kamen creator of the Segway is seeking a patent for an inflatable wind turbine. Kamen makes it clear he does not see this as a game-changing energy generator. Instead, he views it more as a neat way to create a little power and perhaps an outdoor messaging system.
 
The idea for inflatable wind turbines is not a new idea. The Company "Magenn" is currently working on a dirigible like "Air Rotor System." However Dean Kaman's invention does not have tethered like the Magenn system.
image
The Megenn turbine
 
Kamen explained, “The inflatable sail wind turbine may be installed in various locations that a heavier and/or larger conventional wind turbine may not (be), for example … on the roof of buildings.”
 
Kamen's patent application shows how the spinning turbine could be used as a persistence of vision (POV) LED system. From the patent : “light emitting diodes … powered by energy generated by the wind turbine, an image on the blades may include, but are not limited to, pictures, text, symbols, numbers, the date and time, weather forecasts, traffic information, and advertising.” It seems like highway billboards may have their days numbered.
 
Eavesdropper
  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 14 years ago

    I wonder if he has also realized that you could use a water filled turbine for use in the ocean and streams.  The beauty of the simplicity is such an elegant solution.  I hope his idea takes off and these devices proliferate.  They could well be the technology to unlock green energy at an economical level.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 14 years ago

    I wonder if he has also realized that you could use a water filled turbine for use in the ocean and streams.  The beauty of the simplicity is such an elegant solution.  I hope his idea takes off and these devices proliferate.  They could well be the technology to unlock green energy at an economical level.

     

    DAB