Power & Energy
  • Technologies
  • More
Power & Energy
Forum RE: MOSFET IGBT Driver UCC27423
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 283 subscribers
  • Views 513 views
  • Users 0 members are here
  • driver
  • igbt
  • ucc27423
  • cfl
Related

RE: MOSFET IGBT Driver UCC27423

billabott
billabott over 14 years ago

...  So to reduce part$ count, I thought it might be possible to have this driver chip with 2 output pins control 3 IGBT gates (normally full off) with output pinA and 1 IGBT gate (normally full on) with the output pinB.  It is my understanding that the gates are very high impedance so it might not make much difference to pinA if it controls one or three gates.  Has anybody done this successfully?  This is my first go around with IGBTs.

-  thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    You are correct.  The gate is high impediance once the switch is on or off, but during the transitions there is current flow to charge/discharge the capacitance of the gate.  That's why you need a gate resistor between your driver chip and the discrete, to control the turn on/off speed.  Look a the spec sheet and you'll see that a smaller Rg results in faster switching (but more EMI). 

     

    So as to controlling 3 IGBTs with one driver output.  Yes it will work, but there may be issues with timing if that is critical in your circuit.  If the IGBTs are different, or the gate resistors are, then they will turn on/off at different speeds possibly causing problems.  Also if you are switching at very high frequency you need to make sure the driver chip can handle the power required. 

     

    If you're running below 10 kHz and all the IGBTs are the same, I would reccommend increasing the Rg from the spec sheet, but other than that it should work just fine.