Power & Energy
  • Technologies
  • More
Power & Energy
Forum Choosing 13.8V to 3.3V Switch Mode Voltage Regulator
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 284 subscribers
  • Views 1026 views
  • Users 0 members are here
Related

Choosing 13.8V to 3.3V Switch Mode Voltage Regulator

e14 Contributor
e14 Contributor over 14 years ago

I'm designing a circuit with some IC's that is supposed to have a 3.3V voltage supply. My voltage source is a 13.8V battery pack. I'm looking for a high efficiency voltage regulator to supply the circuit, but I'm inexperienced in this area and would like some help finding the best solution. The circuit will have a max current of about 300-400 mA.

 

The efficiency of the regulator is extremely important, because the batteries will have to last as long as possible before recharging is necessary.

  • Sign in to reply
  • Cancel
  • RWM
    RWM over 14 years ago

    For best efficiency you need IC which uses synchronous rectification. For example LM3103MH/NOPBLM3103MH/NOPB

    http://www.ti.com/product/lm3103

    Efficiency about 93%. You can use Webench (available on the page mentioned above) to design and simulate your regulator circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to RWM

    Thank you! I will look into it.

     

    The fact that the current in the circuit will normally be about 1-3 mA (there are components that will be switched off when not in use) may be another thing to consider when choosing a voltage regulator. I don't have much room for a heatsink, so that's another reason to get a highly efficient buck converter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • RWM
    RWM over 14 years ago in reply to e14 Contributor

    If the circuit needs normally 1-3 mA, you should use regulator with pulse skipping mode at light loads (or Eco mode etc.) because standard regulators have bad efficiency at light loads. For example you can use http://www.ti.com/product/tlv62150 (efficiency about 80% at 1mA load and about 90% at 400 mA load).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to RWM

    Thank you!

     

    Do you have examples of other usable regulators? That perticular one seems to be hard for me to get a hold of (can't find it in the electronic shops). I've been searching around the web for replacements, but I'm overwhelmed by all the information and parameters that need to be considered.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • RWM
    RWM over 14 years ago in reply to e14 Contributor

    There is a lot of step-down regulators, but you need to find information on low current efficiency, so search datasheets. Perhaps it is posssible to obtain a sample of above mentioned ICs from TI. Other types:

    http://uk.farnell.com/texas-instruments/tps54528dda/buck-sync-adj-5a-8so/dp/2064230?Ntt=tps54528

    Efficiency about 90% at 400mA but about 50% at 3mA.

    http://www.ti.com/product/tps54428

    http://uk.farnell.com/texas-instruments/tps54428dda/buck-sync-adj-4a-8sop/dp/2078519?Ntt=tps54428

    Efficiency about 90% at 400mA but about 45% at 3mA.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • RWM
    RWM over 14 years ago in reply to e14 Contributor

    You can use also LT3695:

    http://www.linear.com/product/LT3695

    http://cds.linear.com/docs/Datasheet/3695fa.pdf

    http://uk.farnell.com/linear-technology/lt3695emse-3-3-pbf/ic-step-down-regulator-msop-16/dp/1783337

    Efficiency about 84% at 400mA and 62% at 3mA.

    or LT3435

    http://www.linear.com/product/LT3435

    http://cds.linear.com/docs/Datasheet/3435fa.pdf

    http://uk.farnell.com/linear-technology/lt3435efe-pbf/ic-switching-reg-adj-smd-tssop16/dp/1273811?Ntt=lt3435

    Efficiency about 85% at 400mA and 72% at 3mA.