Power & Energy
  • Technologies
  • More
Power & Energy
Forum AC and DC power to light a Bulb
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 284 subscribers
  • Views 4294 views
  • Users 0 members are here
Related

AC and DC power to light a Bulb

e14 Contributor
e14 Contributor over 14 years ago

Hello all!  I am trying a small project and I want to use a small solar cell (say 10vdc 500ma for roundish numbers) to supplement lighting up a 60 watt incandescent bulb.  Knowing that wall electricity is AC and solar cells put off DC I don't know how or if the bulb would use the power from the DC cell.  Also I don't want to have the AC power fry the solar cell, so I need to stop AC flow in that direction and I don't want the DC power to go back to the "grid" I want it to go to the light source.  Any thoughts on doing this?  Would I be able to get a lower net energy use if I checked it with a electricy usage devise like a kill-a-watt energy usage measuring devise or would the bulb just still draw the 60 watts and perhaps glow a bit brighter because of the slightly extra DC power? 

 

Would this be any different with a CFL or a LED bulb?

 

I'm not a electronics engineer...just a guy who tinkers so please excuse any major flubs!  Also I KNOW it's not feasable...I really want to make it work though...its fun to me!  Thanks guys! -Ron

  • Sign in to reply
  • Cancel
Parents
  • YT2095
    YT2095 over 14 years ago

    You`re asking a really good question here! and happily it has A simple answer.

    in effect you`re thinking about a DC current with an AC ripple to make up the rest of the power required by the bulb, I like your thinking, but solar cells are awkward in that respect.

    you Are favored by using DC on incandescent bulbs, it`s much "Greener" than AC, by virtue of the fact that the bulbs last longer on DC also.

     

    but your best bet would be to use a battery for storing this electricity  that will be suplemented from the mains power for charging when it`s dark, a simple UPS will do this with minor modifications.

    I use this exact same set-up myself, the nice part is that I still have juice when the rest of the street has none in a blackout 6685.contentimage_2516.png

    Yes you will need to use a Diode in series with your solar panel, and it must never see AC (it won`t charging a battery).

     

    the problem with a solar cell is that it`s somewhat Dynamic, if you can Promise 100% that it will always have 100% sunshine without varying, then it`s a simple circuit, but this isn`t the case, a cloud passing over can end with lighting your bulb Through a solar cell! (a bad thing).

    and anyway, 10v @ .5A is only 5W, so you`de be better off storing that or buying a whole load more.

    LEDs on the other hand will lend themselves quite nicely to battery power at low voltages!

     

    this is just my opinion based on what I have here and use, others may have better ideas 2553.contentimage_3.png

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • YT2095
    YT2095 over 14 years ago

    You`re asking a really good question here! and happily it has A simple answer.

    in effect you`re thinking about a DC current with an AC ripple to make up the rest of the power required by the bulb, I like your thinking, but solar cells are awkward in that respect.

    you Are favored by using DC on incandescent bulbs, it`s much "Greener" than AC, by virtue of the fact that the bulbs last longer on DC also.

     

    but your best bet would be to use a battery for storing this electricity  that will be suplemented from the mains power for charging when it`s dark, a simple UPS will do this with minor modifications.

    I use this exact same set-up myself, the nice part is that I still have juice when the rest of the street has none in a blackout 6685.contentimage_2516.png

    Yes you will need to use a Diode in series with your solar panel, and it must never see AC (it won`t charging a battery).

     

    the problem with a solar cell is that it`s somewhat Dynamic, if you can Promise 100% that it will always have 100% sunshine without varying, then it`s a simple circuit, but this isn`t the case, a cloud passing over can end with lighting your bulb Through a solar cell! (a bad thing).

    and anyway, 10v @ .5A is only 5W, so you`de be better off storing that or buying a whole load more.

    LEDs on the other hand will lend themselves quite nicely to battery power at low voltages!

     

    this is just my opinion based on what I have here and use, others may have better ideas 2553.contentimage_3.png