Power & Energy
  • Technologies
  • More
Power & Energy
Forum AC and DC power to light a Bulb
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 284 subscribers
  • Views 4303 views
  • Users 0 members are here
Related

AC and DC power to light a Bulb

e14 Contributor
e14 Contributor over 14 years ago

Hello all!  I am trying a small project and I want to use a small solar cell (say 10vdc 500ma for roundish numbers) to supplement lighting up a 60 watt incandescent bulb.  Knowing that wall electricity is AC and solar cells put off DC I don't know how or if the bulb would use the power from the DC cell.  Also I don't want to have the AC power fry the solar cell, so I need to stop AC flow in that direction and I don't want the DC power to go back to the "grid" I want it to go to the light source.  Any thoughts on doing this?  Would I be able to get a lower net energy use if I checked it with a electricy usage devise like a kill-a-watt energy usage measuring devise or would the bulb just still draw the 60 watts and perhaps glow a bit brighter because of the slightly extra DC power? 

 

Would this be any different with a CFL or a LED bulb?

 

I'm not a electronics engineer...just a guy who tinkers so please excuse any major flubs!  Also I KNOW it's not feasable...I really want to make it work though...its fun to me!  Thanks guys! -Ron

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    First, remember that the light bulb was designed to function using 120VAC because that is what travels into our homes.  Thus a 60W light bulb is way too much for your 5W solar panel.  To be honest, the light bulb has a filament inside that needs to reach a certain temperature and once it reaches that temperature it will emit visible light!  The light bulb could careless if it was receiving AC or DC current as it just needs current!  If you want to have fun, rip open a solar garden light and google ckt's that match the one you have in your hands.  Be careful as newer ones have a big glob covering the brains of the ckt and you pretty much destroy the chip removing the glob.  My advice, grab a very small solar array, diode, light dependent resistor, npn transistor, and nicad AA battery with LED and you will learn more in 4 hours than you could 2 weeks reading about it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    First, remember that the light bulb was designed to function using 120VAC because that is what travels into our homes.  Thus a 60W light bulb is way too much for your 5W solar panel.  To be honest, the light bulb has a filament inside that needs to reach a certain temperature and once it reaches that temperature it will emit visible light!  The light bulb could careless if it was receiving AC or DC current as it just needs current!  If you want to have fun, rip open a solar garden light and google ckt's that match the one you have in your hands.  Be careful as newer ones have a big glob covering the brains of the ckt and you pretty much destroy the chip removing the glob.  My advice, grab a very small solar array, diode, light dependent resistor, npn transistor, and nicad AA battery with LED and you will learn more in 4 hours than you could 2 weeks reading about it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Ronald,

     

    One very simple rule you need to remember.  Current always travels from higher potential to lower potential.  I have no clue what you are trying to achieve by connecting in series the solar panel with 120VAC other than harming yourself or watching a solar arrays blow up.  This is not like mixing audio files....120VAC is going to drive current directly into your 10V solar panel on the first half cycle and the drive-120VAC on the next half cycle which will reverse polarity.....just be safe in what ever u do