Power & Energy
  • Technologies
  • More
Power & Energy
Forum Fairchild Semiconductor to Focus on Silicon Carbide Solutions at Electronica Europe 2012
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 281 subscribers
  • Views 302 views
  • Users 0 members are here
Related

Fairchild Semiconductor to Focus on Silicon Carbide Solutions at Electronica Europe 2012

e14 Contributor
e14 Contributor over 13 years ago

Hi All

I thought this might be of some interest to the group.....more so if you are actually going to Electronica of course!

In summary, we'll be outlining and demonstrating our solutions for SiC BJTs, LED Lighting, automotive sector, PSUs, smart metering power, motion control, DC-DC with focus on portable power applications.

I'll only be there on Thursday and Friday but we have a small army of technical staff, that would be more than happy to discuss any requirements you might have, on station throughout the event.

 

SAN JOSE, Calif. – October 9, 2012 – Fairchild Semiconductor (NYSE: FCS), a leading global supplier of high performance power and mobile semiconductor solutions, will exhibit the latest in silicon carbide (SiC) technology as well as over 15 innovative power  and mobile solutions in hall A-4, booth 506 at the electronica Europe 2012 show, in the New Munich Trade Fair Centre, Munich, Germany, between 13 – 16 November.

 

Committed to providing solutions and support to designers that lead to opportunities for success, Fairchild will demonstrate the company’s high performance SiC bipolar junction transistor (BJT) technology that enables higher efficiency and higher power density for applications such as solar inverters, welding systems, and mobile power.

 

The Fairchild team will also conduct demonstrations in application areas such as LED lighting, automotive, power supplies, smart meters, motion control and DC-DC conversion, as well as solutions for portable applications, including  portable power management and interface.

 

Featured demos include:

  • LED Lighting:FL6961 single-stage flyback and boundary mode PFC controller; the 1550V FJAFS1510A30V FDC655 single N-channel logic level MOSFET. Also included in demonstrations at the booth is the FL7730 single-stage primary side regulation (PSR) controllerFL7701 smart non-isolated buck LED driver
  • Automotive: A steering sub-assembly demonstration will showcase Fairchild’s latest 40V PowerTrenchRegistered MOSFETs that utilizes Fairchild’s automotive power module (APM) and TO-Leadless packaging technology. Leveraging the APM technology, these devices support the automotive electronic industry’s need for higher currents and power density, lower power dissipation and smaller footprints.  
  • Industrial Power: On display will be a complete solution for industrial power that includes the FOD8316 smart gate driver optocoupler, an advanced 2.5A output current IGBT drive optocoupler comprised of high-speed isolated feedback for fault sensing; and Fairchild’s 650V field stop IGBTs, theFGA40N65SMD and FGA60N65SMD, that feature high current handling capability, positive temperature coefficient, tight parameter distribution and awide safe operating area.
  • Motion Control: Fairchild will demo a complete motion control solution that includes an analog and digital integrated motor controller that provides a powerful motor control algorithm and a flexible user interface in a single-chip design. Included is the FSBB20CH60C, part of Fairchild’s SPMRegistered smart power module family, that provides single-supply IGBT gate driving capability with an integrated high-speed HVIC; the FPSTm FSL206MR integrated PWM controller; and the FCM820x series of three-phase sinusoidal BLDC motors for improved motor drive efficiency.
  • Smart Meter: A smart meter solution demo will include the highly integrated FAN6300 PWM controller suitable for high-frequency operation (up to 190kHz) for flyback converters; as well as Fairchild’s latest uni-directional smart relay drivers with integrated features, such as accurate timer pulses, that will save space, cost and make disconnect solutions safer and smarter.
  • DC-DC Conversion: Fairchild experts will also demonstrate the GreenBridgeTm FDMQ86530L quad-MOSFET with superior thermal regulation designed to dramatically reduce power loss in active bridge applications. Also on display will be Fairchild’s latest mid-voltage Dual CoolTm package technology, ranging from 40-150V, the devices provide exemplary switching performance as well as low junction-to-ambient thermal resistance.
  • Portable: Fairchild will also have on display innovative mobile semiconductor design solutions that lower power consumption, extend battery life, boost on-the-go performance and speed time-to-market.

 

Offering a unique combination of functional, process, and packaging innovation, coupled with exceptional power systems expertise, Fairchild offers high system-level energy efficiencies with advanced power semiconductors, integrated IC solutions and applications expertise. Come by booth 506 in hall A-4 and discuss your 1W-1200W power design challenges.