Power & Energy
  • Technologies
  • More
Power & Energy
Forum what to use for power meterring
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 282 subscribers
  • Views 414 views
  • Users 0 members are here
  • measuring
  • meterring
  • power
  • input/output
Related

what to use for power meterring

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I am developing a product that manages energy for retail application. I need a device that can measure the overall power usage (from a distribution board, and passed through a current transformer) and output a signal that I can read with a microcontroller. Ideally the device would be self powered. I have read that I might need a watt transducer, but I haven't been able to confirm this anywhere. Any thoughts as to where I should look?

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 12 years ago

    Presumably the voltage is fixed and doesn't require measurement. (If it is varying the same type of circuitry may be needed to measure the voltage)

    The current transformer will have an AC output that needs to be rectified to become a DC voltage for your microcontroller. Look for an active rectifier circuit that eliminates diode "drops" that standard bridge rectifiers rob from your output. You may also need to filter the output to create a constant DC signal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 12 years ago

    Presumably the voltage is fixed and doesn't require measurement. (If it is varying the same type of circuitry may be needed to measure the voltage)

    The current transformer will have an AC output that needs to be rectified to become a DC voltage for your microcontroller. Look for an active rectifier circuit that eliminates diode "drops" that standard bridge rectifiers rob from your output. You may also need to filter the output to create a constant DC signal.