Power & Energy
  • Technologies
  • More
Power & Energy
Forum Which Li-Ion IC and is parallel considered multi-cell?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 282 subscribers
  • Views 536 views
  • Users 0 members are here
  • boost
  • li-ion
  • ion
  • lithium
  • converter
  • Design
  • battery
  • cell
  • power
Related

Which Li-Ion IC and is parallel considered multi-cell?

e14 Contributor
e14 Contributor over 11 years ago

I am working on a portable raspberry pi machine that I want powered by 2 18650 batteries. Since everything in the project runs on 5V, I just want the two 4.2v batteries in parallel with a boost converter stepping it up to 5v and powering all of the devices. I want it to be charged via micro USB and I'm considering two IC's for the charging circuit: The LTC4054 or the BQ2056. Datasheet links at the bottom. Both of these datasheets state that they are single cell, which slightly confuses me. What constitutes as multi-cell: having the cells in series, parallel, or both? If I can't link the batteries in parallel, would I just be able to buy two chips and separately charge each battery?(with a slight change of the current wiring setup, of course)

 

Thanks in advance,

 

Tom

 

Datasheets for LTC4054 and BQ2056:

 

http://www.linear.com/product/LTC4054-4.2

 

http://www.ti.com/lit/ds/symlink/bq2056.pdf

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    I would use the LT part since it needs fewer external parts.

    It should be OK with the 2 cells in // but do go through the data sheet carefully.

    It's going to take a long time to charge two 18650 cells if you use ones with good capacity.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago

    I would use the LT part since it needs fewer external parts.

    It should be OK with the 2 cells in // but do go through the data sheet carefully.

    It's going to take a long time to charge two 18650 cells if you use ones with good capacity.

     

    MK