Power & Energy
  • Technologies
  • More
Power & Energy
Forum Energy generator
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 285 subscribers
  • Views 1906 views
  • Users 0 members are here
Related

Energy generator

royston02
royston02 over 11 years ago

This idea was in me for a long time. I know that when stepper motors are rotated, they generate electricity. However they are big and bulky. Which is the smallest thing that generates electricity in oscillatory motion(like stepper motors)?

Minimum amperage - 100-125ma.  Minimum voltage - 5V or high(AC/DC).

  • Sign in to reply
  • Cancel

Top Replies

  • kidiccurus
    kidiccurus over 11 years ago +1
    Hmm, I don't know the voltage but a regular DC motor might do the job, especially with the help of some gearing. It is also possible that some piezoelectric material could do the same. How fast and with…
Parents
  • dougw
    dougw over 11 years ago

    DC motors are most often used for this application, but they need to be geared up so they rotate many times per step. As mentioned, the power they generate is mostly not free despite many attempts to capture just the wasted part of walking energy. The power they generate makes it more work to walk - the more power they generate, the harder it is to walk.

    Another popular method uses Piezo-electric generators. These can be simpler to design and pretty efficient, but it is tough to get much power at the frequency of stepping - they work much better at high vibration frequencies. They pretty much need a method of mechanically translating a stepping frequency to a high frequency vibration. They generate the same amount of charge every time they are flexed, so to generate more charge (current) they need to flex more often.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 11 years ago

    DC motors are most often used for this application, but they need to be geared up so they rotate many times per step. As mentioned, the power they generate is mostly not free despite many attempts to capture just the wasted part of walking energy. The power they generate makes it more work to walk - the more power they generate, the harder it is to walk.

    Another popular method uses Piezo-electric generators. These can be simpler to design and pretty efficient, but it is tough to get much power at the frequency of stepping - they work much better at high vibration frequencies. They pretty much need a method of mechanically translating a stepping frequency to a high frequency vibration. They generate the same amount of charge every time they are flexed, so to generate more charge (current) they need to flex more often.