Power & Energy
  • Technologies
  • More
Power & Energy
Forum Digital Current/Voltage Control
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 285 subscribers
  • Views 2184 views
  • Users 0 members are here
  • power
Related

Digital Current/Voltage Control

kas.lewis
kas.lewis over 11 years ago

I am looking to control the current/voltage to a device using a microcontroller. The essence of what I am trying to do is control a TEC so that a block of copper/aluminum is kept at an approximately stable temperature. To do this I would like to use a microcontroller running some form of feedback loop that is reading data from a temperature sensor or two and based on that controlling the TEC. I am still looking whether it is the voltage or current that controls the TEC temperature differential but I thought I would get a head start with trying to answer this question which really should not be so hard since I'm sure I have learned this stuff at one point. Anyways thanks for the help in advance.

 

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago in reply to kas.lewis +2
    Hi Kas, Shabaz has done a good job of covering the bases. Also PWM is built into the Arduino and I suspect the other boards as well so it is an easy choice. Using it to control your FET will put the power…
  • jw0752
    jw0752 over 11 years ago +1
    Hi Kas, I just took a Peltier and slowly increased the voltage across the junction. As I raised the voltage the current followed in a fairly linear fashion. Of course as the voltage and current got higher…
  • shabaz
    shabaz over 11 years ago +1
    Hi Kas! I think John is saying that although you could measure current and try to adjust the voltage so that the current through the peltier can be adjusted, it appears to be linearly related to the voltage…
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Kas!

     

    I think John is saying that although you could measure current and try to adjust the voltage so that the current through the peltier can be adjusted, it appears to be linearly related to the voltage anyway. So by varying the voltage, you are varying the current linearly.

    PWM can be considered like an average voltage across the device, so it is a nice way achieving control if it suits your scenario. The reason PWM is often preferred (generally - I have very little knowledge of peltier devices : ( is because it is efficient (little power wasted - if linear control was used, then there would be power loss in the transistor or device used to cause some voltage drop, and that loss could be significant since peltier devices usually pass a fair amount of current - e.g. John's peltier device can take 2A at 6V, which is a lot of power 2x6=12W and then the heat in the transistor would also then need to be taken into consideration). Some control algorithm would still be needed, just that the output of it would control the PWM ratio, not an analog control.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago

    Hi Kas!

     

    I think John is saying that although you could measure current and try to adjust the voltage so that the current through the peltier can be adjusted, it appears to be linearly related to the voltage anyway. So by varying the voltage, you are varying the current linearly.

    PWM can be considered like an average voltage across the device, so it is a nice way achieving control if it suits your scenario. The reason PWM is often preferred (generally - I have very little knowledge of peltier devices : ( is because it is efficient (little power wasted - if linear control was used, then there would be power loss in the transistor or device used to cause some voltage drop, and that loss could be significant since peltier devices usually pass a fair amount of current - e.g. John's peltier device can take 2A at 6V, which is a lot of power 2x6=12W and then the heat in the transistor would also then need to be taken into consideration). Some control algorithm would still be needed, just that the output of it would control the PWM ratio, not an analog control.