Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is this circuit good for watching a 5V battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 282 subscribers
  • Views 1490 views
  • Users 0 members are here
  • battery_analyzer
  • 5v
Related

Is this circuit good for watching a 5V battery?

tim687
tim687 over 11 years ago

Goodmorning everybody,

 

Recently I've purchased a powerbank for my Arduino and I need to check if the powerbank is running low on power (at runtime).

 

I've found a example of a 12V voltage circuit: http://www.janspace.com/b2evolution/arduino.php/2010/06/26/scooterputer

 

I suppose when the lights go red, the battery is dying, and need to be replaced/charged. I want to make such a thing for my 5V powerbank, but can I use the same resistors?

 

If not, can you show my how to calculate the resistance values for the resistors, so that I can do it right in the near future?

 

 

Thank you in advance,

 

Tim

  • Sign in to reply
  • Cancel
Parents
  • peterjcs23
    0 peterjcs23 over 11 years ago

    Tim, if your Suuply voltage is VSup, RA is the 10k reistor, RB is the 4.7k resistor then VAn is the voltage applied to the analog input in the link you gave us, then the equation is:

     

    VAn = VSup (RB/(RA+RB))

     

    with the original numbers VAn is 12 (4.7/(10+4.7)) = 3.84V, which is the voltage the software will detect to put the light on

     

    with VSup=5V, VAn will be 1.60V

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • peterjcs23
    0 peterjcs23 over 11 years ago

    Tim, if your Suuply voltage is VSup, RA is the 10k reistor, RB is the 4.7k resistor then VAn is the voltage applied to the analog input in the link you gave us, then the equation is:

     

    VAn = VSup (RB/(RA+RB))

     

    with the original numbers VAn is 12 (4.7/(10+4.7)) = 3.84V, which is the voltage the software will detect to put the light on

     

    with VSup=5V, VAn will be 1.60V

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tim687
    0 tim687 over 11 years ago in reply to peterjcs23

    Thanks!!

     

    I'll write down the formula and use it next time!

     

     

    Do you think I've got plenty of range? So if the VSup is low because it's empty, do you think VAn won't be 0 V?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • peterjcs23
    0 peterjcs23 over 11 years ago in reply to tim687

    You need to decide what is the minimum voltage at which your circuit works correctly but you need to warn about the battery. If the battery drops too low then the circuit stops working and you can't run the monitor anyway. For example, If say 3V is the minimum working VSup then your monitor software will be looking for VAn input of 0.96V.