Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is this circuit good for watching a 5V battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 282 subscribers
  • Views 1490 views
  • Users 0 members are here
  • battery_analyzer
  • 5v
Related

Is this circuit good for watching a 5V battery?

tim687
tim687 over 11 years ago

Goodmorning everybody,

 

Recently I've purchased a powerbank for my Arduino and I need to check if the powerbank is running low on power (at runtime).

 

I've found a example of a 12V voltage circuit: http://www.janspace.com/b2evolution/arduino.php/2010/06/26/scooterputer

 

I suppose when the lights go red, the battery is dying, and need to be replaced/charged. I want to make such a thing for my 5V powerbank, but can I use the same resistors?

 

If not, can you show my how to calculate the resistance values for the resistors, so that I can do it right in the near future?

 

 

Thank you in advance,

 

Tim

  • Sign in to reply
  • Cancel
Parents
  • artful_bodger
    0 artful_bodger over 11 years ago

    The 2 resistor circuit is called a potential divider and is used in lots of places in electronics.  This link http://www.electronics2000.co.uk/calc/potential-divider-calculator.php is to a calculator, so you can play with the resistor values to get the output voltage you want.

    I'd check with the manufacturer of the powerbank to see if they specify a minimum voltage, as most types of battery are permanently damaged (aka life shortened) by continual discharge to a too low a voltage. You might even find your powerbank shuts itself down, to protect the battery, once it can no longer keep the USB 5V line within specification, which IIRC is 4.75V.  This would mean you need to shut down at say 4.9V to give yourself a bit of margin on ADC and reference errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 11 years ago in reply to artful_bodger

    Thanks!

    I'll lookup the voltage for various battery charges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tim687
    0 tim687 over 11 years ago in reply to artful_bodger

    Thanks!

    I'll lookup the voltage for various battery charges.