Power & Energy
  • Technologies
  • More
Power & Energy
Forum PC PSU usage
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 286 subscribers
  • Views 938 views
  • Users 0 members are here
  • pc
  • heat_extraction
  • supply
  • power
Related

PC PSU usage

scorpion
scorpion over 10 years ago

I have a power supply out of an old tower computer that I want to use for a project. When I fire up the supply the fans in it make a lot of noise. If I remove the fans, will I have any danger of overheating in a wooden enclosure with 2+ inches of space on each side and 2 two inch holes in the wood?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • pcmorris
    pcmorris over 10 years ago in reply to scorpion +3
    Ben, I don't think anyone should give a straight yes answer to this question as getting it wrong is dangerous. Ultimately you really need to look at how much power your going to be dissipating in the device…
  • johnbeetem
    johnbeetem over 10 years ago +2
    I wouldn't take out all the fans. Power supplies usually have a few key components that get quite hot, and if you don't have enough air flow bad things could happen. However, you may not need all the fans…
  • DAB
    DAB over 10 years ago +1
    Hi Ben, Sometimes the old PSU power supplies buzz when there is a short circuit. Others have a positive connection required with the motherboard that needs to be made before they will work. Make sure you…
Parents
  • DAB
    0 DAB over 10 years ago

    Hi Ben,

     

    Sometimes the old PSU power supplies buzz when there is a short circuit.

    Others have a positive connection required with the motherboard that needs to be made before they will work.

     

    Make sure you get a users guide for the power supply so you know exactly what you are dealing with.

     

    Assuming the unit still works, you can then wire it up, make sure you keep the fans and then check the voltage outputs under load conditions.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scorpion
    0 scorpion over 10 years ago in reply to DAB

    DAB,

    I have checked all function of the PSU and confirmed they work. I was just wanting to remove the fans because they are making the noise.

     

    Thanks,

    Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pcmorris
    0 pcmorris over 10 years ago in reply to scorpion

    Ben,

     

    I don't think anyone should give a straight yes answer to this question as getting it wrong is dangerous. Ultimately you really need to look at how much power your going to be dissipating in the device to calculate what the temperature is like in the worst case operation. Obviously the designer of your tower assumed the unit needed forced cooling, however if your running at a reduced load this might not be the case for you. You could try running your setup without the box to gauge the temperature, fit a new fan to the unit or design additional hardware for thermal protection. The idea of running something hot in a flammable box always makes me twitchy, I would definitely not want to do leave anything I was uncertain about running unattended next to dry timber. Probably not a very useful response sorry but just be careful.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pcmorris
    0 pcmorris over 10 years ago in reply to scorpion

    Ben,

     

    I don't think anyone should give a straight yes answer to this question as getting it wrong is dangerous. Ultimately you really need to look at how much power your going to be dissipating in the device to calculate what the temperature is like in the worst case operation. Obviously the designer of your tower assumed the unit needed forced cooling, however if your running at a reduced load this might not be the case for you. You could try running your setup without the box to gauge the temperature, fit a new fan to the unit or design additional hardware for thermal protection. The idea of running something hot in a flammable box always makes me twitchy, I would definitely not want to do leave anything I was uncertain about running unattended next to dry timber. Probably not a very useful response sorry but just be careful.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • pcmorris
    0 pcmorris over 10 years ago in reply to pcmorris

    Just to add im not recommending you work on it outside of an enclosure if that exposes you to live wiring, I assume the psu is probably enclosed but if its not, have it enclosed safely while live.