Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging with low power
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 25 replies
  • Answers 4 answers
  • Subscribers 287 subscribers
  • Views 4641 views
  • Users 0 members are here
  • charging
  • battery_charger
  • low_power
  • battery
  • lipo
  • wireless
  • coil
  • tesla_coil
  • low_power_charger
  • low_power_supply
Related

Charging with low power

balearicdynamics
balearicdynamics over 10 years ago

If I charge a LiIon 500 mA 3.7 V battery with a charger that has a 100 mA power only, the battery will be charged in a longer time or not charged at all ?

 

Thanks in advance to solve this doubt.

 

Enrico

  • Sign in to reply
  • Cancel

Top Replies

  • amgalbu
    amgalbu over 10 years ago +3 suggested
    The charge processo of a LiPo battery has two phases Constant current: the voltage is kept to 4.2 V and current flows into the battery. The charger tries to keep current constant Constante voltage: when…
  • jonivanart
    jonivanart over 10 years ago in reply to balearicdynamics +1
    ambrogio is correct on the requirements the charger should be able to meet. I kinda got all technical on my answer so I hope it wasn't too confusing. LOL! Please mark a good answer if it was answered correctly…
  • crjeder
    crjeder over 10 years ago in reply to jonivanart +1
    Balancing is only needed when multiple cells are charged. This is because a cell which is carged to a lower voltage is the charged by an other cell with higher voltage and the current is not limited. A…
  • jonivanart
    0 jonivanart over 10 years ago

    Hello Enrico!

    First off, the rating of mA on the battery is the max discharge rate.

    Secondly, the LiIon battery has to be charged with a monitoring and balance charger built specifically for LiIon batteries. Please "DO NOT" use just any power source to charge any batteries. LiPoly's. NiMh, NiCad, etc. all require specific types of chargers and methods. The charger will ask to set the voltage due to the balancing feature if the battery has multiple cells or just one. It will also ask for the mH of the battery pack. This is also to charge at a specific rate that is required for that type of cell. 

     

    Lastly, the rating on the power source is also the max power output rating.

    Side note: If you want to get the most out of your battery packs look up "Storage Voltage" of that type of cell. When you want to put them on the shelf for a while, make sure you bleed them down or charge them up to that voltage to make them last or they will go bad on the shelf.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to jonivanart

    Hi Jon,

     

    thank you for the warning. This is something I almost know but unfortunately I am not a big expert (nor a small image ) in the calculation of the battery systems. I'll try to be more specific.

     

    The battery is the following in the image below, with the listed characteristics:

    image

    LiPo rechargeable battery, 500mA/h, 3.7 V, 48x20x4 mm dimensions

     

     

    I plan to use a coil inductance recharger like the one shown in the image below:

    image

    Generating an output regulated voltage of 3.7 or 5V with 100-300 mA power and - as far as I know (declared by the producer) it should charge single-cells LiPo batteries.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jonivanart
    0 jonivanart over 10 years ago in reply to balearicdynamics

    I could see charging single cells. Just keep in mind that there is a percentage charge rate. The voltage is most important as far as fully charging the battery. Even that voltage is a certain amount of the rating of the battery cells.

    As far as the rate of charge (Amperage) it needs to be a certain amount of the discharge rate. It has been a while so I can't remember off hand what that is on certain cells but a quick Google can get you that info.

     

    Basically it works like this:

    Charge rate = % of discharge rate (mAh) and cell type

    Top off charge (Full charge) = voltage + but not more than a certain percentage over voltage capacity of the cell type

     

    With the type of of charging you are asking about you will need to regulate the voltage and charge rate. The closer you get to max charge rate the faster it will charge but you risk damaging the cell and it does shorten the life of the cell the closer you get also. Another words the slower (The lower the charge rate) the better it is for the cell. Like most things heat is the enemy. The faster the charge the more heat generated. ;-)

     

    Hope this helps...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 10 years ago

    The charge processo of a LiPo battery has two phases

    Constant current: the voltage is kept to 4.2 V and current flows into the battery. The charger tries to keep current constant

    Constante voltage: when the battery voltage reaches the applied voltage, current drops

    So to answer tour question: to fully charge tour battery it would take a shorter or longer time depenfing on the current tour charger fan supply ad far the charger voltage is 4.2 V

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to amgalbu

    Hi Ambrogio!

     

    Thank you for your suggestion. That's what I was supposing. So with a lower power supply charger for me it is not matter if the charge time is a bit longer.

     

    BTW, the wireless charging seems not possible due the dimensions of the coil that will require a too large size of the device box.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jonivanart
    0 jonivanart over 10 years ago in reply to balearicdynamics

    ambrogio is correct on the requirements the charger should be able to meet. I kinda got all technical on my answer so I hope it wasn't too confusing. LOL!

    Please mark a good answer if it was answered correctly so that the post can be marked as a solved issue.

    Thanks...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to jonivanart

    Jon, don't worry, I have idea of how it works. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to balearicdynamics

    Would be nice to have a document handy for such knowledge!image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to clem57

    What do you mean exactly Clem?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • crjeder
    0 crjeder over 10 years ago in reply to jonivanart

    Balancing is only needed when multiple cells are charged. This is because a cell which is carged to a lower voltage is the charged by an other cell with higher voltage and the current is not limited. A to hig charge current will destroy the battery cell. That's why you have to do balancing while charging multiple cells.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>