Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar Panel system to keep seldom-used truck battery charged
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 284 subscribers
  • Views 489 views
  • Users 0 members are here
  • automobile
  • charge controller
  • solar
Related

Solar Panel system to keep seldom-used truck battery charged

e14 Contributor
e14 Contributor over 10 years ago

Hello all!

 

I have a pickup truck that I only drive maybe once or twice a week. Sometimes a week will pass between uses. I bought a NOCO 2.5W solar panel kit to keep it topped off and it does OK, but during this cloudy and cold winter I had to charge the battery once with an external charger.

 

So I'm thinking that I need a larger solar panel. I can mount it in the bed of the truck, right behind the cab, pointing straight up. (I plan to hinge the mounting so I can just fold it up to make room for anything I need to haul in the truck, and to protect it.)

 

I'm looking for ideas as to how much of a panel I need and should I incorporate a PWM charge controller, and maybe any other automotive specific things I might need to know.

 

Thanks for any input you can give me!

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    A different idea: use mirrors and position carefully to increase the lumens on the current solar cells.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mzungu
    0 mzungu over 10 years ago

    clarkdv For this kind of application, where we can assume that the battery is fully charged after you drive the vehicle, I would go for a 15 or 20 Watt panel.  Even with this small current, there is still the possibility of over-charging the battery - so some kind of control is needed.  I would not bother with a PWM charge controller - what you really want to do is limit the charging voltage to 13.8 to 14 V.  The current from a 20W panel in the brightest sun should not exceed 2A (more likely 1A) so I would just use a zener diode to dump the excess into a resistive load.  There are 3A rated controllers (for about 10 to 15 USD) that do this, but they tend to limit at 14.2V, which is a bit on the high side.  Don't forget you will need a (Schottky) diode to prevent the battery discharging into the panel at night!