Power & Energy
  • Technologies
  • More
Power & Energy
Forum Low voltage cut-off circuit for hub dynamo
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 282 subscribers
  • Views 701 views
  • Users 0 members are here
  • low voltage cut-off
  • uvlo
  • low voltage power management
  • under voltage lockout
Related

Low voltage cut-off circuit for hub dynamo

bobanr
bobanr over 8 years ago

I want to design a circuit which receives power from a 6V,3W hub dynamo and boost it before supplying it to a LiPo battery. I want to cut-off the output from the hub till 3.3V and supply the output to the booster only above 3.3V. At present, I have an XL6009 DC-DC converter. I want to know if it's possible to design a standalone circuit or if a specific device is available for this purpose.

  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago

    The data sheet for the XL6009 chip is available and states that it needs a minimum input voltage of 5V - so it isn't really suitable for your purpose.

    There are boost converters that will work with lower input voltages.

    The XL6009 and most other such chips has a an enable control which you could drive with  a suitable ciruit to make sure that it only runs when the input voltage is above a threshold,  but you need a different chip for 3V input.

    Are you able to design and make circuit boards or are you looking for a ready made solution ?

    What is the battery voltage and how do you control charging ?

     

    MK