Power & Energy
  • Technologies
  • More
Power & Energy
Forum using a battery powered motor to charge a battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 283 subscribers
  • Views 1764 views
  • Users 0 members are here
  • Alternative Energy Tags
  • battery
  • kenetic energy
  • energy
Related

using a battery powered motor to charge a battery

crusinex
crusinex over 8 years ago

so i have been thinking about energy harvesting using a battery powered motor running clockwise on a wheel and having another motor running counter clockwise on the other side of the wheel charging a secondary battery while the primary battery is running.

 

is this possible to fully charge a secondary battery while a primary battery is powering the first motor?

 

the motors would be separated by the wheel therefore no electrical currents would be being drained from one battery to the other, just the mechanical energy transfer

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +6 suggested
    Yes it is possible to do this, but it would take more energy from the first (discharging) battery than you would add to the second (charging) battery. There are losses in the wires, in the motor and in…
  • dougw
    dougw over 8 years ago in reply to crusinex +4 suggested
    Good thought but unfortunately it doesn't improve efficiency. A gearbox can increase the output speed, but it correspondingly reduces the amount of torque so you can't get more total power out. And as…
  • dougw
    dougw over 8 years ago in reply to crusinex +3 suggested
    for car batteries roughly... you lose: 10% of discharging battery energy as heat less than 1% heating wires about 5% in the motor from friction and IR losses about 4% from friction in gears if you have…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Conner,

    You might try searching the site for motor charging battery as we have had similar discussions in the past and you might glean some more information and insights from them.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago

    Hi Conner,

    You might try searching the site for motor charging battery as we have had similar discussions in the past and you might glean some more information and insights from them.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer