Power & Energy
  • Technologies
  • More
Power & Energy
Forum using a battery powered motor to charge a battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 283 subscribers
  • Views 1762 views
  • Users 0 members are here
  • Alternative Energy Tags
  • battery
  • kenetic energy
  • energy
Related

using a battery powered motor to charge a battery

crusinex
crusinex over 8 years ago

so i have been thinking about energy harvesting using a battery powered motor running clockwise on a wheel and having another motor running counter clockwise on the other side of the wheel charging a secondary battery while the primary battery is running.

 

is this possible to fully charge a secondary battery while a primary battery is powering the first motor?

 

the motors would be separated by the wheel therefore no electrical currents would be being drained from one battery to the other, just the mechanical energy transfer

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +6 suggested
    Yes it is possible to do this, but it would take more energy from the first (discharging) battery than you would add to the second (charging) battery. There are losses in the wires, in the motor and in…
  • dougw
    dougw over 8 years ago in reply to crusinex +4 suggested
    Good thought but unfortunately it doesn't improve efficiency. A gearbox can increase the output speed, but it correspondingly reduces the amount of torque so you can't get more total power out. And as…
  • dougw
    dougw over 8 years ago in reply to crusinex +3 suggested
    for car batteries roughly... you lose: 10% of discharging battery energy as heat less than 1% heating wires about 5% in the motor from friction and IR losses about 4% from friction in gears if you have…
Parents
  • dougw
    0 dougw over 8 years ago

    Yes it is possible to do this, but it would take more energy from the first (discharging) battery than you would add to the second (charging) battery. There are losses in the wires, in the motor and in the batteries than make the process less than 100% efficient. It might be more efficient to directly charge the second battery from the first, but there would still be losses that make it less than 100% efficient.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • crusinex
    0 crusinex over 8 years ago in reply to dougw

    what if i use gears to make the secondary motor spin faster than the primary (discharging) motor?

     

    i know there would still be a loss in energy via heat and friction but would that make the the transfer of power more efficient or at least compensate for the difference in energy?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to crusinex

    Good thought but unfortunately it doesn't improve efficiency. A gearbox can increase the output speed, but it correspondingly reduces the amount of torque so you can't get more total power out. And as you point out there are also more losses in the gearbox.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • crusinex
    0 crusinex over 8 years ago in reply to dougw

    so what would the amount of energy loss be from my original idea?

     

    would it be a 20% loss from heat and friction?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to crusinex

    for car batteries roughly... you lose:

    • 10% of discharging battery energy as heat
    • less than 1% heating wires
    • about 5% in the motor from friction and IR losses
    • about 4% from friction in gears if you have some
    • about 10% in the generator from friction and IR losses
    • about 10% in charging the second battery as heat

    nowhere do you gain energy in this system - the second battery stores some fraction of the energy (roughly 60%) supplied by the first battery

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • crusinex
    0 crusinex over 8 years ago in reply to dougw

    so for a 33v/51ahr lithium ion battery being charged id only be getting 19.8v?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • crusinex
    0 crusinex over 8 years ago in reply to dougw

    so for a 33v/51ahr lithium ion battery being charged id only be getting 19.8v?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • genebren
    0 genebren over 8 years ago in reply to crusinex

    The battery would likely charge very close to 33V, but the total charge might be closer to ~30ahr.  The voltage relationship to charge is not linear.  The battery rapidly rises to near it's terminal voltage, but charge (Ahr) is much more linear.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer