Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging 4 3.7V LiPo batteries in parallel with wireless induction charging model.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 282 subscribers
  • Views 860 views
  • Users 0 members are here
  • wireless charging
  • li-ion or li-po battery
Related

Charging 4 3.7V LiPo batteries in parallel with wireless induction charging model.

btellefsen
btellefsen over 8 years ago

Same concept as a tooth brush charger. I am stepping down 120V to 5V, with full wave rectifier and 1000uF capacitor. I'm very familiar with making transformers just not as familiar with wireless charging. I am using the stepped down power to charge 4 - 3.7V 750mAh LiPO batteries in parallel. What would be the best way to regulate battery charging, protect against over/uneven charging?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi Blake, Keep in mind that the rectifier and capacitor (which is probably not needed for the NiMH battery in the toothbrush) are on the toothbrush side. You will need a magnetic field that is varying…
  • jw0752
    0 jw0752 over 8 years ago

    Hi Blake,

     

    Keep in mind that the rectifier and capacitor (which is probably not needed for the NiMH battery in the toothbrush) are on the toothbrush side. You will need a magnetic field that is varying to induce a voltage across a wireless gap. For wireless phone charging they use a higher frequency than the 50 or 60 cps available from the mains as the higher frequency is more efficient. You might want to check out this excellent Road Test by shabaz  that covers a wireless power development board.

     

    https://www.element14.com/community/roadTestReviews/2558/l/wireless-power-design-kit-medium-power-review

     

    This sounds like an interesting project and I look forward to how it turns out.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer