Power & Energy
  • Technologies
  • More
Power & Energy
Forum Dealing With Low Battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 8 answers
  • Subscribers 285 subscribers
  • Views 3297 views
  • Users 0 members are here
  • control
  • battery
  • power
  • solar
  • remote
  • sensor
Related

Dealing With Low Battery

ntewinkel
ntewinkel over 8 years ago

Hi All,

 

I'm hoping to use solar for powering micro controller data logging/sensing projects.

 

Specifically, I have an ESP-8266 (like Adafruit's Huzzah) based project I'd like to run on solar. (the temperature logger I blogged about recently)

 

The ESP, being WiFi enabled, uses a fair bit of power to communicate, and I would like to avoid any issues with brownout or shutdown at bad times. And also perhaps issues with startup/shutdown flickering.

 

The challenges include:

1. charging a battery from the solar panel.

2. output of the battery has to provide 3.3v to power the board

3. battery should be sufficiently charged before it provides power to the board

4. battery should shut down the board (cut the power) when voltage goes too low

5. The micro controller should be super energy efficient - ie, sleep most of the time, wake up just long enough to do something, then sleep again.

 

I'm still having trouble wrapping my mind around points 3 and 4.

 

Mark mcb1 suggested:

>For the Forget me Not challenge, the EnOcean devices reduced their reporting rate to suit the charge they had.

 

Which is a great idea - dynamically adjusting sleep and wake times depending on battery voltage. But I think it only addresses part (most) of the concerns.

 

My more direct concern with 3 and 4 was more outside of the control of the microcontroller: can we keep the battery controller from providing any power at all until a minimum threshold is achieved? ie, if battery pack voltage drops to the minimum 3.2volts, shut off power to the microcontroller, and then don't provide power again until it's back up to, say, 3.4 volts. I suppose a very power-miser type controller could control that part (digispark maybe?). So the battery would need enough power to run the digispark, and the digispark would turn on a relay if it figures there's enough power to run the ESP8266. I'm pretty sure I've seen battery protection circuits out there that will avoid over-discharge that can shut off power to the digispark in those cases.

 

I guess there's also that detail about not cutting power to the ESP when it's in the middle of communications.

 

Thanks,

-Nico

 

ps, This discussion started in another thread, but I thought it could use its own spot, mostly for future reference for all of us image

 

pps, The rough approach is to just set it up and hope it doesn't run out of power much, and else just let it deal with it, but I'm looking for a gentler more refined solution.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +5 suggested
    ntewinkel I ran across this post on the LowPowerLab site. https://lowpowerlab.com/2017/09/15/weathershield-supercapacitor-tiny-solar-cell/ Using a supercap might be an alternative. Mark
  • mcb1
    mcb1 over 8 years ago +4 verified
    Seems you need this https://www.adafruit.com/product/3428 A voltage detector is handy for projects where you want to make sure your microcontroller doesn't run at a low voltage. For example, say you have…
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +4 suggested
    Hi Raymond, Thanks for that link. It looks like a more general 12volt kind of setup. I've done that before with bigger panels and a controller, charging a bank of 12v batteries. Unfortunately the panels…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    Seems you need this

    https://www.adafruit.com/product/3428

     

    A voltage detector is handy for projects where you want to make sure your microcontroller doesn't run at a low voltage. For example, say you have a Feather Huzzah running on a lipoly battery every few minutes. Eventually the battery runs down, and goes below 3.3V, so the voltage to the ESP8266 core is too low, and could cause a lockup or corrupted data. Or maybe your battery is already drained and you're trying to charge it back up, but as you are trying to charge it up, the Huzzah turns on and the spike of current drains the battery immediately so it never gets through the trickle-charging stage.

    This little chip is a simple solution: It monitors the voltage on one Input pin, and when that voltage goes below 3.3V, it will pull the  Output pin low. If you connect that Output pin to the Enable pin on the Feather, it will make sure that the Huzzah does not run if the battery dips too low.

     

    Adafruit have a number of Lipo cells that have over and under voltage cutouts.

    This one cuts out at 3v.

    https://www.adafruit.com/product/258

     

    They talk mostly about 5v charging, and I haven't really seen a 3v3 output device.

    This one does have the status available, so you could use it to shutdown the ESP.

    https://www.adafruit.com/product/390

     

     

    I would suggest if you have spare I/O, then signal when your sending (or when it's safe to shutdown) and use the controller/voltage monitor to shut it down.

     

    Let me know when you get it sorted ... I'll copy it image

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    Seems you need this

    https://www.adafruit.com/product/3428

     

    A voltage detector is handy for projects where you want to make sure your microcontroller doesn't run at a low voltage. For example, say you have a Feather Huzzah running on a lipoly battery every few minutes. Eventually the battery runs down, and goes below 3.3V, so the voltage to the ESP8266 core is too low, and could cause a lockup or corrupted data. Or maybe your battery is already drained and you're trying to charge it back up, but as you are trying to charge it up, the Huzzah turns on and the spike of current drains the battery immediately so it never gets through the trickle-charging stage.

    This little chip is a simple solution: It monitors the voltage on one Input pin, and when that voltage goes below 3.3V, it will pull the  Output pin low. If you connect that Output pin to the Enable pin on the Feather, it will make sure that the Huzzah does not run if the battery dips too low.

     

    Adafruit have a number of Lipo cells that have over and under voltage cutouts.

    This one cuts out at 3v.

    https://www.adafruit.com/product/258

     

    They talk mostly about 5v charging, and I haven't really seen a 3v3 output device.

    This one does have the status available, so you could use it to shutdown the ESP.

    https://www.adafruit.com/product/390

     

     

    I would suggest if you have spare I/O, then signal when your sending (or when it's safe to shutdown) and use the controller/voltage monitor to shut it down.

     

    Let me know when you get it sorted ... I'll copy it image

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to mcb1

    Great finds, Mark! Thanks image

     

    I didn't know about voltage detectors, but that's a neat little gadget. I have a Huzzah here (part of a shopping cart contest prize image), and I see it has the enable pin. The other ESP boards don't have it, so it looks like Adafruit added some smarts to their boards.

     

    It looks like the easiest solution is to just purchase the Adafruit solar kit = battery + solar panel + charging board. And +voltage detector and Huzzah. Not the cheapest, but with Adafruit you know it's done well.

     

    But when have you ever known me to take the easy route?  ok well... Mac, Arduino, RPi... but besides those times (and ignore the electric bicycle assist too)... And ok I admit I have lots of little easy to use modules for all kinds of specific purposes...

     

    But I digress, ignore that last line.

     

    I'm wondering what the enable pin on the Huzzah does, and if that can be generalized to other boards.

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to ntewinkel

    >I pondered:

    >I'm wondering what the enable pin on the Huzzah does, and if that can be generalized to other boards.

     

    Thought I'd read up on the Huzzah some more, and found this:

     

    EN (CH_PD) - This is the enable pin for the ESP8266, pulled high by default. When pulled down to ground momentarily it will reset the ESP8266 system.

     

    Which corresponds to a pin on the ESP chip itself, and it looks like other boards simply call it RST. And even the very limited ESP-01 has the ch_pd pin.

     

    So it's ok to hold a board in extended reset? Which is what Adafruit seems to suggest:

    "If you connect that Output pin to the Enable pin on the Feather, it will make sure that the Huzzah does not run if the battery dips too low."

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to ntewinkel

    So it's ok to hold a board in extended reset?

    I beleive there may have been a similar discussion when jw0752 was doing his thing with the battery timer.

     

    The trick would be if the particular micro goes into a low current mode while it's held low.

    Presumably the clock is dead, and all the outputs are also low or tri-state.

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer