Power & Energy
  • Technologies
  • More
Power & Energy
Forum question about decoupling capacitor
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 283 subscribers
  • Views 776 views
  • Users 0 members are here
  • decoupling capacitor
Related

question about decoupling capacitor

houandreas
houandreas over 8 years ago

hi,I'm learning from one schematic from a mezzanine card and designing a PCB for my own project. I found that on that schematic there are decoupling capacitors for power supply 3.3V and Vadj but none for the power supply 12V. On that Schematic the 3.3V is used to supply the IIC but 12V is not used. But it might be used for other high frequency IC right? So why it doesn't get a decoupling capacitor, I can't understand.

 

I'll convert the 12V to 5V to supply my 2x16 character LCD,  the connections which I saw online never contains a decoupling capacitor. Is it because the LCD already have a decoupling capacitor in itself?

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 8 years ago +1 verified
    Hello, have a look at this Decoupling Tutorial by Analog Devices . Although there are CMOS circuits that can work with 12 V, logic circuits are rarely powered with this voltage. The most common are 5 V…
Parents
  • koudelad
    0 koudelad over 8 years ago

    Hello,

     

    have a look at this Decoupling Tutorial by Analog Devices. Although there are CMOS circuits that can work with 12 V, logic circuits are rarely powered with this voltage. The most common are 5 V, 3,3 V, 2,5 V and 1,8 V. As you mentioned, 3,3 V in your case.

     

    The LCD module you mention definitely has some capacitors, they need to be as close to the power pins as possible, so they can't rely on the designer of a custom board.

     

    David

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • koudelad
    0 koudelad over 8 years ago

    Hello,

     

    have a look at this Decoupling Tutorial by Analog Devices. Although there are CMOS circuits that can work with 12 V, logic circuits are rarely powered with this voltage. The most common are 5 V, 3,3 V, 2,5 V and 1,8 V. As you mentioned, 3,3 V in your case.

     

    The LCD module you mention definitely has some capacitors, they need to be as close to the power pins as possible, so they can't rely on the designer of a custom board.

     

    David

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer