Power & Energy
  • Technologies
  • More
Power & Energy
Forum Convert toy motor to Solar Power - where to begin?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 1080 views
  • Users 0 members are here
Related

Convert toy motor to Solar Power - where to begin?

drmikeg
drmikeg over 8 years ago

Following a visit to the Amazing MAD museum in Stratford, UK - my Son saved his allowance to buy a "glow in the dark rail race" kit.

image

Which is so brilliant, he hasn't actually let me play much with it yet.

It has an Archimedes screw, driven via a reduction gearbox (which I've not looked at yet) from a motor powered by a single C cell battery.


My only complaint about this great kit is that the motor and gearing is OUTRAGEOUSLY noisy given what is does. It's sounds more like its driving a compressor!

So, I'd like to convert the motor to optionally run (much slower) from a small solar cell.

It can then sit on the shelf, and periodically, during daylight, marbles will set off.

 

I'll continue to do my own research, but does anyone have any tips? (I suspect once I find the right solution, it won't prove very complicated)

 

My first thought is some form of Juele-thief circuit, with a diode with a 1.5V on-voltage?

Many thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • danielw
    danielw over 8 years ago +6 suggested
    We went MAD museum Last month over Easter. It's amazing! I got the much smaller wooden marble run... For myself, I think my wife thought I was the biggest child! Especially when I started tweeting a box…
  • drmikeg
    drmikeg over 8 years ago +3 suggested
    I'm going to link here to this amazing project: https://www.element14.com/community/community/project14/solarpowerdevices/blog/2018/08/07/solar-bubble-blaster Many thanks
  • mcb1
    mcb1 over 8 years ago +3 suggested
    I liked the one in Fracture where Anthony Hopkins plays the lead role. This was the opening credits https://www.youtube.com/watch?v=Y-v6E9H6nh0 It was designed by a Dutch artist Mark Bischof. https://www…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    I liked the one in Fracture where Anthony Hopkins plays the lead role.

    This was the opening credits

    https://www.youtube.com/watch?v=Y-v6E9H6nh0

     

     

    It was designed by a Dutch artist Mark Bischof.

    https://www.youtube.com/watch?v=HZB7FpXX30w

     

     

    Apparently you can have a tour.

    https://adutchexperience.com/events/gravity-random-and-rolling-balls-in-kinetic-art/

     

     

    They have some in Australia and you can buy them (at fairly expensive prices)

    Rolling Ball Sculpture - Kinetic rolling ball sculptures designed and created by David Morrell

     

     

     

    But back to your issue.

    The gearbox is the item making the noise, so changing the motor is unlikely to fix this problem.

    Solar powered is simply a lot weaker, and may not even power it.

    The motor will still require gearing, but you may be able to use a motor and gearbox combined.

     

    I'd suggest investigating the gearbox to determine what is causing the noise.

    It could be a lack of lubrication, and one of the best things you can do is measure the motor current while trying to determine what is loading it.

     

    Assumming it is running well, it could simply be transferring the movement into one of the surfaces, which is translating that into the sound.

    Poking or prodding these should show what is the source.

     

     

    I note that the structures in the movie used a large wheel to transfer the balls to the top.

    This is certainly a far more efficient way to do it, and is likely to use less power and be silent.

    Perhaps some design and 3D printing, or some woodworking might solve it.?

     

    Mark.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • drmikeg
    0 drmikeg over 8 years ago in reply to mcb1

    Hi Mark,

     

    Thanks for the reply.

     

    I will investigate the gearbox, and together with some suggestions from the solar-bubble-blaster thread, I'll post an update with any progress I make.

     

    Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drmikeg
    0 drmikeg over 8 years ago in reply to mcb1

    Hi Mark,

     

    Thanks for the reply.

     

    I will investigate the gearbox, and together with some suggestions from the solar-bubble-blaster thread, I'll post an update with any progress I make.

     

    Thanks