Power & Energy
  • Technologies
  • More
Power & Energy
Forum What could cause MAX17552 to switch the LX pin only at 8% duty cycle when the FB pin reads 100mV?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 5 answers
  • Subscribers 282 subscribers
  • Views 1229 views
  • Users 0 members are here
Related

What could cause MAX17552 to switch the LX pin only at 8% duty cycle when the FB pin reads 100mV?

tomattila
tomattila over 8 years ago

I have small auxiliary power supply around a MAX17552 DCDC IC.

 

Pins:

- IN connected to 25V

- EN/UVLO connected to 25V

- RT/SYNC pulled to ground by 68kohm (reads 350mV)

- SS open

- MODE open

- 330pF capacitor on RESET

- VOUT grounded

- 100uH inductor connected to LX, the output capacitor is 10uF. (LX on-time appears to be 0.5uns, the off-time is 6.5 us)

- GND grounded

- FB gets the output voltage divided by 220K and 33K (reads 100mV)

 

And here comes the problem:

Even though the FB pin reads 100mV, the LX pin is only switching at 8% so the output votlage is only around 800 mV, instead of the expected 6.1V. What can cause this? Is there maybe a current limit on the LX pin?

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 8 years ago +3 suggested
    LX on-time appears to be 0.5uns, the off-time is 6.5 us That would imply an output of 1.8V. Are you sure it isn't also doing some pulse skipping? From the datasheet, it looks as if your problem may relate…
  • tomattila
    tomattila over 8 years ago +3 suggested
    Finally I decided to completely take apart the board. Sure enough there is nothing wrong with the MAX17552 circuit. There is a 1EDN7512G gate driver on the board and the official eagle library from Infineon…
  • genebren
    genebren over 8 years ago +2 suggested
    Greetings, Without seeing the schematic (yes, your description is fairly clear), or knowing the test conditions (load or no load), it is difficult to tell what is going wrong. As best I can tell, it seems…
Parents
  • genebren
    0 genebren over 8 years ago

    Greetings,

     

    Without seeing the schematic (yes, your description is fairly clear), or knowing the test conditions (load or no load), it is difficult to tell what is going wrong.  As best I can tell, it seems that you have things connected correctly (it almost matches the example in the specification).  What load are you testing at?  The LX pin is limited to 0.21A. Did you verify the DC resistance and saturation current ratings of your inductor?

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • genebren
    0 genebren over 8 years ago

    Greetings,

     

    Without seeing the schematic (yes, your description is fairly clear), or knowing the test conditions (load or no load), it is difficult to tell what is going wrong.  As best I can tell, it seems that you have things connected correctly (it almost matches the example in the specification).  What load are you testing at?  The LX pin is limited to 0.21A. Did you verify the DC resistance and saturation current ratings of your inductor?

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • tomattila
    0 tomattila over 8 years ago in reply to genebren

    Thanks. Tried no load and 100ohm load. There seems to be no difference in behavior. The inductor is a Coilcraft LPS3015-104M (100uH, 0.24A saturation current). I think it should be fine but somehow it isn’t. I’ll try inductors with higher inductance and higher current rating next week.