Power & Energy
  • Technologies
  • More
Power & Energy
Forum stepper motor power needs
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 790 views
  • Users 0 members are here
Related

stepper motor power needs

kobedie
kobedie over 8 years ago

i need stepper motors and have been wondering if it would be better to use a 5kg/cm or a 4Kg/cm motor.

They are rated 2.5A and 1.7A respectively. I wanted to use just a regular meanwell psu. is it better to go with the higher torque one and why?

i need the highest torque but am limited in power.

nema 17 models mentioned:

 

2.5A:     SL42S247A

1.7A:     42BYGHW609L20P1X2

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +3 verified
    You could always dial the high torque/high current device back when high torque is not needed and save power that way. It would provide high torque when needed but low power when high torque is not needed…
  • kobedie
    kobedie over 8 years ago in reply to dougw +1
    is true, tough i will see in the shop if the bigger psu fits. if so i will use the highest rating possible for future iddirations.
Parents
  • dougw
    0 dougw over 8 years ago

    You could always dial the high torque/high current device back when high torque is not needed and save power that way. It would provide high torque when needed but low power when high torque is not needed. It might complicate your power supply though. If you don't need high holding torque, you might turn motor power right off when they aren't moving.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kobedie
    0 kobedie over 8 years ago in reply to dougw

    is true, tough i will see in the shop if the bigger psu fits. if so i will use the highest rating possible for future iddirations.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kobedie
    0 kobedie over 8 years ago in reply to dougw

    is true, tough i will see in the shop if the bigger psu fits. if so i will use the highest rating possible for future iddirations.