Power & Energy
  • Technologies
  • More
Power & Energy
Forum Potentiometer for LCD
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 285 subscribers
  • Views 2688 views
  • Users 0 members are here
Related

Potentiometer for LCD

houandreas
houandreas over 8 years ago

hi, I'm searching a potentiometer for the contrast control of an LCD. One side of it should be connected to 5V and the other to GND. The middle pin will be connected to V0 which adjusts the resistance. However, I found that the power rating of most potentiometers in market is just 50mW with the minimal resistance of them is 50 Ohm. Assuming the potentiometer works at extreme condition which is 50 Ohm and the voltage on it is 5V. The power it consumes would be 5x5/50=0.5W  >>50mW. It would be unacceptable.  There is 0.5W potentiometer in the market but it's rare, so I guess I'm thinking this wrong. Does anyone have any clue for such condition?  Thanks!

 

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +5 verified
    This is the normal configuration. The Pin simply receives a voltage and there is little or no current drawn. At the upper end it will receive 5 volts, 2.5v at the middle and 0v at the lower end. Mark
  • mcb1
    mcb1 over 8 years ago in reply to houandreas +5 suggested
    I was so stupid I don't think that is correct. You asked relevant questions, and more importantly gave enough information for us to work out how you were connecting it, and verify it wasn't an issue. Stupid…
  • beacon_dave
    beacon_dave over 8 years ago +3 suggested
    Try using a 10k pot instead ? https://www.arduino.cc/en/Tutorial/HelloWorld
Parents
  • mcb1
    0 mcb1 over 8 years ago

    This is the normal configuration.

    image

    The Pin simply receives a voltage and there is little or no current drawn.

    At the upper end it will receive 5 volts, 2.5v at the middle and 0v at the lower end.

     

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • houandreas
    0 houandreas over 8 years ago in reply to mcb1

    I was so stupid... my connection is just as you showed in that diagram. I know that the resistance can be changed by changing the position of the wiper. But I was thinking the resistance is between supply and GND.(resistance between supply and GND is fixed at 10k).  thank you. I was thinking in the wrong direction....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • houandreas
    0 houandreas over 8 years ago in reply to mcb1

    I was so stupid... my connection is just as you showed in that diagram. I know that the resistance can be changed by changing the position of the wiper. But I was thinking the resistance is between supply and GND.(resistance between supply and GND is fixed at 10k).  thank you. I was thinking in the wrong direction....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 8 years ago in reply to houandreas

    I was so stupid

    I don't think that is correct.

    You asked relevant questions, and more importantly gave enough information for us to work out how you were connecting it, and verify it wasn't an issue.

     

    Stupid would be not asking the question. image

     

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer