Power & Energy
  • Technologies
  • More
Power & Energy
Forum Horsepower to Watts
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 284 subscribers
  • Views 1772 views
  • Users 0 members are here
  • alternative power
  • hydrogen
  • engine
Related

Horsepower to Watts

ericcb
ericcb over 8 years ago

Hello. I am new here. I was told to come here regarding my Prototype CPU Cooler. I am an independent researcher that is struggling. All the engineering firms, or factories I have called, refuse to work with me because I am not a business. I am hoping this is a place I can ask my questions. It is a 2 step problem

First step is the OxyHydrogen. I am using it to get Horsepower. To protect the prototype, I am going to avoid saying how. I hope you can understand. The part I am stuck on is the 4%. The flame is cooler the less Hydrogen there is per volume. The minimum is 4%. Do I increase or decrease the flame nozzle to achieve this? Or is it a container issue? Or both?

The second step involves the engine itself. It will produce horsepower if I can get the 4% figured out. I don't know what the best approach is to using that horsepower, to get the coolant the power it needs. The coolant in question is a refrigeration compressor. I would have to re-design it to work with the engine, or find a way to send electricity to the terminal. Which approach should I take?

These are all the questions I have for now. Any information you can provide is greatly appreciated. Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +4 suggested
    Sounds to me like the University of Canterbury beat you a long time ago and have commercialised it. Whispertech was the commercial arm who developed it for commercial sales. Basically they designed and…
  • jw0752
    jw0752 over 8 years ago +3 suggested
    Hi Ericcb, The first step is going to have to be a rephrasing and detailing of your question. For example your question about the 4%. I am guessing that you are talking about fuel to oxygen percents but…
  • michaelkellett
    michaelkellett over 8 years ago in reply to ericcb +3 suggested
    It's quite easy to design a gas burner where the hot part of the flame is not in contact with any part of the burner. https://en.wikipedia.org/wiki/Bunsen_burner The tube is made of quite normal steel…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    Sounds to me like the University of Canterbury beat you a long time ago and have commercialised it.

    Whispertech was the commercial arm who developed it for commercial sales.

    Basically they designed and built a small, run on anything, power plant.

    In reality it could be used to power/drive anything, but electricity was seen as commercially viable.

     

    For your ratios there is some information here.

    https://en.wikipedia.org/wiki/Oxyhydrogen

     

    and horsepower v watts is

    https://en.wikipedia.org/wiki/Horsepower

     

    With 2 Horsepower you'll have 1450 watts give or take a few available.

    The torque to start the compressor will be the issue, and the output my require gearing or large flywheel to operate without stalling.

     

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    Sounds to me like the University of Canterbury beat you a long time ago and have commercialised it.

    Whispertech was the commercial arm who developed it for commercial sales.

    Basically they designed and built a small, run on anything, power plant.

    In reality it could be used to power/drive anything, but electricity was seen as commercially viable.

     

    For your ratios there is some information here.

    https://en.wikipedia.org/wiki/Oxyhydrogen

     

    and horsepower v watts is

    https://en.wikipedia.org/wiki/Horsepower

     

    With 2 Horsepower you'll have 1450 watts give or take a few available.

    The torque to start the compressor will be the issue, and the output my require gearing or large flywheel to operate without stalling.

     

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ericcb
    0 ericcb over 8 years ago in reply to mcb1

    What you mean University of Canterbury beat me to it? I did a Google search and I am not seeing anything. I am well aware that others in the past, have used OxyHydrogen in a Generator but, I am not doing a generator. I am wanting to power the compressor directly

    I will keep that in mind as I go through different tests. Thank you