Power & Energy
  • Technologies
  • More
Power & Energy
Forum Grounding of secondary for 24vdc power supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 281 subscribers
  • Views 883 views
  • Users 0 members are here
Related

Grounding of secondary for 24vdc power supply

clarkc
clarkc over 8 years ago

Does anyone know of any problems with the grounding of the secondary on the TDK Lambda power supply  DLP75-24-1/EDLP75-24-1/E and  DLP120-24-1/EDLP120-24-1/E The primary voltage is 208 VAC and secondary 24VDC one used to supple the CPU the other for I/O

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +1 suggested
    Cliff, From looking at the TDK DLP Installation manual, I see nothing that would make me believe that there would be a problem tying the grounds together on the two supplies. The only connection that they…
  • genebren
    0 genebren over 8 years ago

    Cliff,

     

    From looking at the TDK DLP Installation manual, I see nothing that would make me believe that there would be a problem tying the grounds together on the two supplies. The only connection that they do not permit is paralleling two supplies (+ to + and - to -).

     

    Here is a link to this manual: https://uk.tdk-lambda.com/KB/DLP-Installation-Manual.pdf

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer