Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC inverter doesn't power on Playstation4 when car is running. Why?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 8 answers
  • Subscribers 284 subscribers
  • Views 6987 views
  • Users 0 members are here
Related

DC inverter doesn't power on Playstation4 when car is running. Why?

iizeroxii
iizeroxii over 7 years ago

I have a dc inverter more than capable enough of powering the PlayStation 4. it works fine when the car is not running. When I start the car so the battery doesn't go flat the PS4 can't power on.

The vehicle is a Chrysler 300c 2013

the inverter is an Energizer 500W: https://www.energizerpower.com/product/en548/

Any idea as to why?

Would a capacitor/stiffening cap help?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago +5 suggested
    Hi Gavin, When the car is off the battery is a solid 12.6 volts and has a very low internal resistance so hooking up the inverter does not cause the voltage to drop much. When the car is running the alternator…
  • Gough Lui
    Gough Lui over 7 years ago +5 suggested
    As a rule of thumb, you should not have anything attached to the lighter socket during cranking. It's a bad idea since the transient from the starter motor can result in much lower and higher voltages…
  • iizeroxii
    iizeroxii over 7 years ago +4 suggested
    Ok so I found the problem. While the inverter was fine for the job. I agree that it should not be used while turning the engine. That was not the problem. The problem was that it doesn't work when the…
Parents
  • iizeroxii
    0 iizeroxii over 7 years ago

    Ok so I found the problem.

    While the inverter was fine for the job. I agree that it should not be used while turning the engine. That was not the problem. The problem was that it doesn't work when the engine is on. So the problem ended up being the AC output wave form was Modified sine wave. I got at new inverter that has pure sine wave and all is good. Thanks for the help people.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to iizeroxii

    I suspect your inverter might have had problems with its protection thresholds if it won't run while the car is running. The output waveform is rarely an issue for most appliances as they use a switching converter anyway. I suspect it's more the fact you got a new inverter that probably doesn't have the fault with regards to protection voltage levels that solved the issue - not the output waveform.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 7 years ago in reply to Gough Lui

    I don't think necessarily the inverter may have issues -maybe- since he found a solution with a new inverter that produces a pure sinewave. My best guess is that the PS4 requires pure sinewave same as some PCs (or some PSU) -I didn't find official confirmation, but see the last comment-. Simulated stepped sinewave may work for some but most of the time people go against the factory recommendations to save money, is not the case here but I didn't find official documentation to support the PS4 power requirements.

     

    If interested here a very quick comparison between the 3 different waveforms which may apply to the inverters as well.

     

    Luis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 7 years ago in reply to Gough Lui

    I don't think necessarily the inverter may have issues -maybe- since he found a solution with a new inverter that produces a pure sinewave. My best guess is that the PS4 requires pure sinewave same as some PCs (or some PSU) -I didn't find official confirmation, but see the last comment-. Simulated stepped sinewave may work for some but most of the time people go against the factory recommendations to save money, is not the case here but I didn't find official documentation to support the PS4 power requirements.

     

    If interested here a very quick comparison between the 3 different waveforms which may apply to the inverters as well.

     

    Luis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer